Subscribe

Latest Blog Post

How food manufacturers in Europe are automating palletizing without adding headcount

Alessio Cappellaro
by Alessio Cappellaro. Last updated on Apr 07, 2026
Posted on Apr 07, 2026 in Palletizing
4 min read time

Across Italy and the DACH region, food manufacturers are facing the same reality:

  • 📈 Increasing production demand
  • 👷 Labor shortages and rising costs
  • ⚠️ End-of-line processes limiting throughput

And more often than not, the bottleneck isn’t where you think.

👉 It’s palletizing.

 

The challenge: Scaling without hiring

chocolate snacks

A premium Italian manufacturer of chocolate, pastries, and snacks recently faced this exact situation.

Their setup was simple — but limiting:

  • 1 operator per palletizing station
  • €40,000/year labor cost
  • 1 shift, 1 line

Scaling production meant only one thing:
➡️ Hiring more operators

But in today’s labor market, that’s:

  • Expensive
  • Unreliable
  • Hard to sustain long-term

So they asked a better question:

👉 “How can we increase output without increasing labor?”

The application: typical (and challenging) food industry constraints

This wasn’t a niche use case. It’s exactly what many manufacturers deal with daily:

  • 📦 Cardboard boxes up to 17 kg
  • ⚡ 6–10 picks per minute
  • 📏 Pallets up to 1,700 mm
  • 🧩 Interlayers required
  • 🔄 Boxes arriving via conveyor, consistently oriented

In other words:

👉 Too demanding for manual scaling
👉 But traditionally seen as too complex for flexible automation

The solution: Robotiq Lean Palletizing (PE20 model)

PE20-1

Instead of going with a rigid, high-cost automation system, the manufacturer selected:

👉 Robotiq PE20

Because it’s designed specifically for manufacturers who need:

✅ Fast deployment

No major layout changes. No long integration cycles.

✅ Safe collaboration

Operate without fencing — ideal for existing production environments.

✅ flexibility

Handle multiple SKUs, box sizes, and pallet patterns without re-engineering.

✅ Ease of use

Operators can run the system without robotics expertise.

The results: Immediate ROI and scalable growth

💰 €40,000 saved per year — per station

By removing one manual palletizing role:

  • Labor costs dropped instantly
  • Payback became highly predictable

📈 Increased throughput

With a stable pick rate of 6–10 picks/min:

  • No more end-of-line bottlenecks
  • Production can scale with confidence

📦 Better pallet quality

  • Consistent stacking
  • Integrated interlayer handling
  • Reduced product damage

🔄 Future-proof operations

As production evolves:

  • New products? No problem
  • New formats? Easily configurable
  • New demands? Already covered

Why this matters for Italian & DACH manufacturers

If you’re running a food production line in:

🇮🇹 Italy
🇩🇪 Germany
🇦🇹 Austria
🇨🇭 Switzerland

You’re likely dealing with:

  • High labor costs
  • Workforce shortages
  • Pressure to increase efficiency

👉 The reality:
Manual palletizing doesn’t scale anymore.

👉 The opportunity:
Automation doesn’t have to be complex or risky.

The smartest first step in automation

Many manufacturers think they need to automate entire lines.

But in reality:

👉 Palletizing is often the fastest, lowest-risk entry point into automation

  • Quick ROI
  • Minimal disruption
  • Immediate impact

Is your application a good fit?

Not every palletizing setup is the same.

The real question is:

👉 Will this work for your boxes, your rates, your layout?

Try the Palletizing Fit Tool (2 Minutes)

Get a clear answer instantly:

  • ✔️ Check if your application is compatible
  • ✔️ Estimate ROI based on your inputs
  • ✔️ Get a recommended configuration

👉 Start your evaluation now with the Palletizing Fit Tool

 

Screenshot 2025-09-08 at 9.41.29 AM