Electric servo grippers offer a different set of functionality than pneumatic grippers. They trade speed and force for flexibility. In fact having specifications such as programmable; stroke, force and speed can make your applications a lot easier. To figure out for which applications is this useful, read on.
For assembly tasks an electric gripper can be really useful. In fact, most assembly tasks are done at a single spot in the production line. This means the gripper that is positioned there must be flexible and be able to grasp different parts. There is absolutely no time for tool changing and this is why a flexible electric gripper should be used.
Also, grippers such as our 3-Finger Adaptive Gripper that have a programmable stroke can reduce the cycle time of the robot considerably. Especially since if you can set the stroke, the gripper doesn't need to run through its whole stroke before closing back on the object. The gripper can be set a little wider than the part and this can reduce the cycle time of the robot by reducing the gripper's motion.
Another interesting aspect of the electric gripper is that it can have embedded sensing. This means you can have direct feedback as to whether or not the part has been grasped by the gripper. This can determine the difference between a productive assembly and a badly integrated assembly.
Another aspect that is often overlooked is your environment. In machining operations, there could be a lot of fluids involved. Since this can effect the functionality of your robot gripper, you have to choose a tool that can work well under your conditions. Irregardless of the type of gripper you choose, the IP rating should be known to make sure your gripper can handle your working environment.
Laboratories or metrology rooms might require clean air environments. By using pneumatic grippers, the air can be contaminated. Some grippers are specifically clean room rated and are designed to be installed in these kinds of rooms. A good alternative to the pneumatic gripper might be an electric on-off gripper. This kind of gripper has the same functionality without the disadvantage of air contamination.
In the same way grippers that are used in laboratories might have to handle fragile parts such as tubes and trays. This means that the gripper probably requires programmable force, which can be done with an electric gripper. In fact, force is just a setting that can be changed in the gripper program to select the gripper grasping force which can be slight or firm depending on the part. In the case where the lab is using a pneumatic gripper, the force has to be set by adjusting the air pressure. However, if the pressure is not constant throughout the actionable time, then force could be higher or lower than necessary which could cause problems for the application.
For more in-depth information on the advantages of electric servo grippers take a look at this ebook.