Subscribe

Latest Blog Post

Improve Robotic Welding Applications with Seam Finding and Tracking

Catherine Bernier
by Catherine Bernier. Last updated on Dec 19, 2024
Posted on Aug 22, 2013 in Robotic Welding
4 min read time

Welding is one of the first manufacturing applications to have been automated in industry. Its complexity and the fact that it is a hazardous job has made it the perfect application to give to industrial robots. Since this time, a lot of other robotic applications have been robotized. In some previous posts, we have talked to you about how vision systems improve actual robotic applications by giving eyes to robot arms. Well, robotic welding also follows this trend, since through the help of vision, welding applications can be improved for even better results.

Seam Finding

seam-tracking-finding-joint-welding-industrial-roboticsThis system allows the robot to precisely locate the joint that will be welded using the two parts as references. Different techniques exist to locate the joint.

The first one needs contact with the part in order to locate the joint; it is called tactile sensing. It uses the welding wire or another wire to touch the part and determine the best position for the weld. For some kinds of welds such as lap welds, it can be used only with material thicker than 3 mm.

The second technique uses a laser point to locate the work surface. This technique is non-contact and significantly faster. This technique can be used with thinner materials than with touch sensing.

The third technique uses laser cameras. They project a laser line which detects both walls at the same time. Moreover, they can reduce cycle time and provide data about joint gap.

Seam Tracking

This system is meant to track the weld position, in real time, during welding. It provides better quality welds, better path speed, optimal weld path and reduced cycle time. Moreover, it can simplify the programming, since the robot will be guided by the system.

This sensing technology looks like the one used for seam finding. It can use tactical sensing, as well as optical sensing.

Tactical sensing has the advantage of not being sensitive to weld splatter or extraneous light. It is the simplest to use. The system will detect if there is any deviation between the edge it touches and the programmed path. The welding wire or a separate wire can be use as a sensor.

Optical tracking moves over the seam, in advance, to detect any deviation from the programmed path. It often uses lasers or cameras.

Control

When a deviation is detected, the robot has to compensate for this deviation. To do so, there are two kinds of control scheme: robot-controlled seam tracking and adaptive seam tracking.

For the first method (robot-controlled seam tracking), the robot controller will receive the data and send the corrections to the robot. Its advantages are to have a reduced device overhead and a smaller shape for the processing head.

welding-automation-kinetiq-control

For the second one (adaptive seam tracking), the robot is mounted with an autonomous processing head that can be programmed independently. So, when a deviation is detected, the data will be sent to this autonomous device that will then determine the compensation. This control scheme is independent from the robot controller and can react fast.

welding-automation-kinetiq-teaching-robotics

These tools can greatly improve your welding application, so that it always produces an optimal weld each time. Ask your robotic welding integrator about which solution would best suit your production parameters.

---

When talking about robotic welding, manual welders are a great asset for companies due to their welding knowledge and expertise. However, when it comes time to automate the welding process, they might become overwhelmed with all the programming. Robotiq has consider this and developed an intuitive solution for the programming required with robotic welding. Kinetiq Teaching is a device that helps people, with no in-depth knowledge of programming, set up their welding robot real fast. Watch the video to see how it works!

COMPARE SPECIFICATIONS FOR 31 WELDING ROBOTS  RIGHT HERE

Leave a comment

Catherine Bernier
Written by Catherine Bernier
Catherine is an Application Engineer here at Robotiq. Drawing from her expertise with manufacturing processes, production management and business management in general, her main focus is helping her clients find the solutions that will best serve their needs. If you have any questions about Robotiq's products and how they can serve your application, get in touch with her at c.bernier@robotiq.com.
Connect with the writer:

Related posts

What is Included in Robotic Welding Systems?

Considering getting into robotic welding? This article should help you wrap your head around robotic welding systems. What's...

Mathieu Bélanger-Barrette
By Mathieu Bélanger-Barrette - October 29, 2014
What is the Cost of a Robotic Welding Cell?

If you're considering buying your first robotic welder, the first question that you have in mind is probably: How much will...

Mathieu Bélanger-Barrette
By Mathieu Bélanger-Barrette - September 22, 2014
Easy Robotic Welding at IMTS in Yaskawa Motoman Booth

IMTS (International Manufacturing Technology Show) is held in Chicago this week. Our Kinetiq Teaching technology is being...

Mathieu Bélanger-Barrette
By Mathieu Bélanger-Barrette - September 11, 2014