Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

Robotic Machine Tending: Advantages and White Paper!

Catherine Bernier
by Catherine Bernier. Last updated on Jul 11, 2022 8:57 AM
Posted on Jun 13, 2013 10:51 AM. 3 min read time

Nowadays, the constant pressure of productivity and cost efficiency are part of the manufacturing industry. In order to stay in business, manufacturers have to find more and more ways to always improve their production line. Automating the fabrication process already exists, but how to save more time and money on the line? Robotic machine tending should be the next step in production line automation.

 

 

Reduce cycle time

Even if the fabrication is automatic, a worker is often needed to feed those machines. The pace of production is still controlled by the pace of a human. Using a robot to do machine tending will save a little time each cycle. Saving a few seconds per cycle, may result in a significant increase in production over weeks and months. Moreover, a robotic tending device can process work 24 hours a day, 7 days a week without tiring.

Save money

Talking about cycle time, it has a direct relation to your production costs. Also, labor costs can go down substantially, because one worker can take care of more than one robot. A machine tending robot would also be less expensive than a specially designed feeding device and it is more flexible, since it can be adapted to more than one type of piece. Combined with a flexible Robot Gripper, no more extra tooling is needed.

Save space

Manufacturers often think that a machine tending robot has to be placed in front of the machine. On the contrary, the robot can be installed overhead and can even serve two machines at a time. Robots tend to be more compact and flexible, they can therefore be installed inside the machine (for big CNC machine of course!). This will save a lot of space on the shop floor.

Cons to consider

Even if there are a lot of advantages to having a machine tending robot, some cons have to be considered. The initial cost of the robot is usually high, from $100,000 to $250,000. Moreover, the robot needs maintenance unlike a human. Also, the robot will not do visual inspection of the piece when unloading the machine. However, a vision inspection system costs about $15,000 to $50,000.

Give flexibility to your machine tending robot

Robotiq 3F gripper loading a part in a CNC lathe

Some say: that a disadvantage might be that a robot can have a hard time handling different types of pieces, we at Robotiq, say: this isn't true. Combining the robot with an electric end effector from Robotiq will give the flexibility needed to insure a fast ROI by eliminating expensive tooling and fixturing. The Robotiq Electric Grippers mechanically intelligent fingers can adapt to any size and kind of object. Since no more changeover is needed, your production costs and time will be reduced.

For more information: Machine tending

Banner of the Robotiq Machine Tending bundle

Leave a comment

Catherine Bernier
Written by Catherine Bernier
Catherine is an Application Engineer here at Robotiq. Drawing from her expertise with manufacturing processes, production management and business management in general, her main focus is helping her clients find the solutions that will best serve their needs. If you have any questions about Robotiq's products and how they can serve your application, get in touch with her at c.bernier@robotiq.com.
Connect with the writer:

Related posts

What's New In Robotics?  07.12.2018

-UR celebrates 10 years since 1st sale-China robot production data -World's first automated ferry -Hello Bennu-Elowan the...

Emmet Cole
By Emmet Cole - December 7, 2018
Demo Week Highlights

What's trending on DoF this week? Demo week kick-off, circle move looped twice, security planes, use of Arduino to control...

Amanda Lee
By Amanda Lee - February 9, 2017
Trending on DoF This Week - Nov. 17

What's trending on DoF this week? Using one snapshot position to sort multiple parts, sampling rate for polishing, Revtech...

Amanda Lee
By Amanda Lee - November 17, 2016