Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

ROS-Industrial: open-source software in industrial robotics

Nicolas Lauzier
by Nicolas Lauzier. Last updated on May 05, 2016 5:15 PM
Posted on Jan 31, 2014 2:00 AM. 3 min read time

A couple years ago Southwest Research Institute (SwRI) released an open-source software package which brings industrial robotics into ROS (Robot Operating System). The stack, as is called a ROS collection of packages, is named ROS-Industrial and is distributed under the BSD license, which basically means that it can be used freely in proprietary (commercial) softwares.

What is ROS and ROS-Industrial?

ROS is a software framework which provides a set of functionalities needed in the development of robot controllers. It allows an easier programming of systems including multiple components (computing nodes, sensors, actuators, ...), as it takes care of various low-level functions such as message-passing between the different sub-systems. On top of that, users can contribute by producing stacks which implement functions needed by many applications. Stacks are currently available for computer vision, mapping, path planning, etc. This allows robot engineers to realize cutting-edge applications by building on the work of others. At the moment, ROS in mainly used for research applications in fields such as autonomous robots, but ROS-Industrial might just change that.

ROS-Industrial is a stack which is intended to ease the integration of ROS into industrial applications. With ROS-Industrial, new nodes that apply to industrial components not necessarily interesting for the research ROS users will be added. SwRI partners with Motoman Robotics and Willow Garage for the development of ROS-Industrial, which tends to illustrate the seriousness of this project. They've so far been able to use ROS to control a SIA10D robot arm for collision-free path planning, as it is shown in this video:

The advantages of open-source software in industrial robotics

The development of ROS-Industrial is very good news for industrial robotics. It is often difficult for robot integrators to build innovative applications from scratch and this is quite easy to understand. Robots are by themselves very complex machines. Imagine now that you have to combine them with other complex, expensive devices to realize novel applications using techniques that noone on your team has experience with. That can be quite scary for small companies that cannot risk failure on any of their projects.

Open-source software, however, has the potential to alleviate the burden of programming complex applications from scratch. Engineers and scientists from research institutes (such as SwRI) and robotics component manufacturers could provide stacks performing simple tasks. The integrators would then combine them together, just like LEGO blocks.

As an example, lets consider the integration of stereo cameras to achieve object recognition and automatic grasping using ROS-Industrial. We're not there yet, but camera suppliers could provide ROS compliant packages for their devices. These packages would be compatible with a standard computer vision library, such as OpenCV from Willow Garage. Another ROS stack, built by others, would be responsible for comparing the data with a catalog of CAD models which are anticipated to be observed by the robot. Finally, another stack would be used to determine the best way to grasp the object. At the end, the integrator would be merely responsible of linking these packages together and customizing the libraries for the specific needs of the application.

How to make this happen?

What I described in the previous section is not happening yet. The question needs to be asked: how can we help foster this open-source software in industrial robotics? Two answers come to my mind:

  • by promoting the production of open-source software in academic research: instead of focusing on publications, professors should also evaluate positively if students spend their time producing reusable open-source software;

  • by making sure that engineering graduates have learned to program using other people's code: too often, they are taught how to reinvent the wheel, whereas it is often more useful to know how to assemble wheels with other components to build cars.

There must be many other ways to promote open-source software, like ROS in the industrial world. I would really enjoy hearing your ideas on the subject! In the mean time, take a look at our ROS package to use our grippers. 

Industrial Communication Protocol Cheat Sheet Get it here

Leave a comment

Nicolas Lauzier
Written by Nicolas Lauzier
Senior Product Manager R&D
Connect with the writer:
http://www.robotiq.com

Related posts

The Human View of Robot Workers: What Do Employees Really Think?

Robot workers are transforming the way we work. There is no denying that they are here to stay… but this raises some...

Alex Owen-Hill
By Alex Owen-Hill - February 21, 2023
7 Exciting and Effective Applications for Robotics in Retail

Robotic technology is transforming the retail industry. With robots, retailers of all sizes can automate and streamline...

Alex Owen-Hill
By Alex Owen-Hill - February 17, 2023
10 Robotics Predictions for Trends That Will Dominate 2023

Robots have come a long way since their early days as big, clunky machines that took up vast spaces in factories.

Today, robots...

Alex Owen-Hill
By Alex Owen-Hill - December 20, 2022