Subscribe

Latest Blog Post

15 Assembly Types: Which to Automate and Which to Avoid

Alex Owen-Hill
by Alex Owen-Hill. Last updated on Nov 14, 2024 3:36 PM
Posted on Apr 15, 2022 8:51 AM. 6 min read time

How many different types of assembly tasks are there? And which should you automate?

Assembly is one of the most common categories of tasks that manufacturers choose to automate with robots.

If you're looking to automate an assembly task in your production line, there are a lot of options you could choose from.

Some of these tasks are easy to automate with a robot. They will give quick returns and will have a high impact on your production. Other assembly tasks are more complex and will have a less clear impact on your production.

Let's look at 15 common assembly tasks. We'll examine which are easy to automate with a robot and which can be trickier.

Worker performing an assembly task with a cobot in a manufacture

What are the broad types of manufacturing tasks?

There are dozens of different assembly processes in manufacturing. Many of these processes are possible to automate with a robot.

You can think of there being 2 broad types of tasks in manufacturing:

  1. Process tasks — These involve taking a workpiece and mechanically changing it to add value to it. Examples of process tasks you can automate are machining, 3D printing, and surface finishing.
  2. Assembly tasks These involve taking already-processed parts and fixing them together.

In this article, we're focusing on the second of these.

The 2 types of assembly task

You can also think of there as being 2 categories of assembly tasks:

  1. Permanent joining methods — This is where the assembly operation is, more or less, non-reversible. Examples include welding, brazing, and adhesive bonding.
  2. Mechanical joining methods — This is where the operation is, more or less, reversible. Examples include screwdriving, inserting, and knotting.

You can automate both types of assembly tasks with a robot.

15 common assembly types and tasks

Here are 15 common assembly tasks that might want to automate. Some are easy to automate with a robot while others are slightly harder.

1. Adhesive bonding

Adhesive bonding involves joining two surfaces together with a chemical agent to create a strong bond. The most common example of this is gluing.

As a simple dispensing task, it's quite easy to automate adhesive bonding with a robot.

2. Bolting

Bolting is one of the most common joining methods in manufacturing. It involves screwing a nut and bolt together. The two main types of bolted joints are tension joints and shear joints.

Robotic bolting can be simple (as simple as screwdriving) or more complex if the nut is unfixed.

3. Brazing

Brazing is a process for permanently joining two pieces of metal together. Using a high-temperature flame, you melt a filler metal to fill the join between the two pieces.

Robotic brazing is certainly possible. Like welding, it requires a specialist setup.

4. Cable tying

Cable ties are a quick and easily-reversible method for joining two items together. They are commonly used to join cables and tubes.

The trickiest part of cable tying with a robot is inserting the end initially. One solution could be to use an automatic cable tie gun as an end effector.

5. Clinching

Clinching is a method for joining sheet metal without welding or fasteners. It involves mechanically deforming the metal together to form a strong joint.

Robotic clinching is certainly possible. However, it tends to require large industrial robots and custom tooling.

6. Crimping

Crimping, like clinching, involves joining two or more materials by deforming them. A common example is wire crimping to join a wire to a connector.

Crimping end effectors for robots are not yet widespread, but there are many automatic crimping tools that you could integrate with a robot.

7. Inserting

Inserting is perhaps the first operation you think of when you think about "assembly." It simply involves pushing one part into another to create a mechanical fit.

It's very easy to automate insertion tasks with robots, especially if you use programming features like Spiral Search.

Robotiq Force Copilot insertion node on a Universal Robot teach pendant

8. Knotting

Knots are a way to join rope and other cords together. It is one of the easiest joining methods for us humans to perform.

Tying knots with robots is a very complex task and is the topic of much ongoing research.

9. Magnet fastening

Sometimes, we want to create an assembly join that is easy to reverse and reattach many times. For this, magnet fastening is one of the most common joining methods.

How easy it is to automate your particular magnet fastening task with a robot depends on the specific task.

10. Nailing or stapling

Nailing and stapling assembly tasks both involve driving solid metal, pin-shaped fasteners into two pieces of material.

Robotic nailing is quite common. The task requires a special automatic stapling end effector.

11. Riveting

What's the most interesting assembly task? It's riveting.

Jokes aside, riveting is a common and highly-effective mechanical joining method. It involves driving a metal rivet into two pieces of material and deforming the rivet to create a strong connection.

Robotic riveting is possible with a special riveting end effector.

12. Screwdriving

Screwdriving is one of the most commonly automated assembly tasks.

The robot picks up a screw from an automated screw feeder. It then drives the screw into the workpiece using a screwdriving end effector.

With an off-the-shelf Robotic Screwdriving Solution, you can quickly and easily deploy your own screwdriving robot.

Robotic screw driver and screw feeder from Robotiq mounted on a robot from Universal Robot

13. Soldering

Soldering is used in electronics manufacturing to fix components to circuit boards. A hot soldering iron is held to the metal contacts and solder is melted onto them.

Robotic soldering is an increasingly common form of assembly automation, using a special soldering tool.

14. Staking

Staking involves connecting two components with an interference fit. A metal or plastic "boss" is inserted into a hole. Then, a high force or ultrasound is applied to deform the boss, fixing it firmly into the hole.

There are a few robotic staking solutions, including those using ultrasonic staking.

15. Welding

Welding involves applying heat, pressure, or both, to two metal parts. Solder is then applied to fuse the two metals. It differs from brazing in that the heat is much higher.

Robotic welding is a highly effective application for manufacturers. It offers various compelling benefits over manual welding, including better consistency, less post-weld clean-up, and more efficient use of materials.

Designing for assembly automation: Which to automate

Of all these 15 assembly operations (and any more you might think of)… which should you automate with a robot in your facility?

The basic rule is to pick a task that is:

  • Simple to automate.
  • High impact for your business.

Say that you choose robotic screwdriving— a very common task to automate. You can then look for examples of other manufacturers who have also automated this task with a robot to learn how they did it.

Meet the Screwdriving Solution

Which assembly task will you automate first? Tell us in the comments below or join the discussion on LinkedIn, Twitter, Facebook, or the DoF professional robotics community.

Leave a comment

Alex Owen-Hill
Written by Alex Owen-Hill
Alex Owen-Hill is a freelance writer and public speaker who blogs about a large range of topics, including science, presentation skills at CreateClarifyArticulate.com, storytelling and (of course) robotics. He completed a PhD in Telerobotics from Universidad Politecnica de Madrid as part of the PURESAFE project, in collaboration with CERN. As a recovering academic, he maintains a firm foot in the robotics world by blogging about industrial robotics.
Connect with the writer:
http://alexowenhill.co.uk/

Related posts

Automation First Strategy: How to Win in the Future of Work

The landscape of work and business is constantly changing. Every time a new technology or way of working takes its hold on an...

Alex Owen-Hill
By Alex Owen-Hill - December 13, 2022
The Cost of Automation: Do the Numbers Really Add Up?

It's no secret that automation can have a huge impact on the way you do business. But does the cost of automation match the...

Alex Owen-Hill
By Alex Owen-Hill - December 7, 2022
How to Automate a Task: It's Easier Than You Think

Are there tasks in your business that everyone finds boring? Those tasks that involve just doing the same actions again and...

Alex Owen-Hill
By Alex Owen-Hill - November 25, 2022