Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

How to Configure a Robotiq Device with DeviceNet Communication Protocol

Mathieu Bélanger-Barrette
by Mathieu Bélanger-Barrette. Last updated on Feb 16, 2015 4:50 PM
Posted on Feb 16, 2015 3:50 PM. 7 min read time

Robotiq specializes in robotic hardware devices. However, to take advantage of all the tools available to configure your gripper with your robot or robotic cell it might be helpful to understand the basics about communication protocol setups. It is in this vain that we thought we would show our readers the basics about configuration setups and troubleshooting for the communication protocol, DeviceNet. Since even for us, this is not our specialty, in this article we will refer to websites that can provide you with more in-depth information in communication protocols and that are more equipped to answer your more specific questions.

 

 

For this article we focus on the DeviceNet communication protocol. This language is the most used in the automation market. Note that all our Robot Grippers can be configured with this communication protocol. Since data handling is based on Producer/Consumer technology this makes it robust and efficient.

What is DeviceNet?

DeviceNet is a digital, multi-drop network that connects and serves as a communication network between industrial controllers and I/O devices such as Robotiq devices. Each device and/or controller is a node on the network. As a Producer/Consumer network, it supports multiple communication hierarchies and message prioritization. DeviceNet systems can be configured to operate in a master-slave or a distributed control architecture using peer-to-peer communication. DeviceNet communication protocol has several features to deliver increased productivity through improved process control and information flow:

  • Operates in a master-slave or a distributed control architecture using peer-to-peer communication.

  • Supports both I/O and explicit messaging for a single point of connection for configuration and control.

  • DC power on the network is available to devices with limited power requirements.

  • Reduces connection points and physical size of network.

  • Follows the Open Systems Interconnection (OSI) model, an ISO standard for network communications, so all necessary functions are defined, from the physical implementation to protocol and methodology to communication of control and information data within and across networks.

  • Provides seamless bridging and routing from DeviceNet to other Common Industrial Protocol (CIP) Networks, which currently include Ethernet/IP™ and ControlNet™.

Configure DeviceNet with a Robotiq Device

First of all, the Robotiq devices that are using the DeviceNet communication protocol are the latest versions of the 2-Finger 85 Adaptive Gripper and the 2-Finger 200 Adaptive Gripper. The 3-Finger Adaptive Gripper will be using the same configuration instruction program, however, this device does not require a Universal Controller. 

You need to make sure your controller (if needed) is capable of communicating via DeviceNet. You can identify a Robotiq controller with a DeviceNet communication capability by looking at the last few digits of its name. For example if a Robotiq Universal Controller is DeviceNet ready, its name will be: UNI-CTR-001-DNET. The controller will then have a 5 pin Combicon plug-in capable of receiving the appropriate wires.

DEVICENET

The DeviceNet and Universal Controller use a separate 24V power supply. If you use several devices on your line, make sure your DeviceNet has its own 24VDC power supply. The DeviceNet cable should only be grounded at one spot on the line, but grounding is important. So, make sure to connect the network Shield and Drain wire to an earth ground using #8 AWG wire up to a maximum 3m in length. Also connect the V- conductor (Black Wire) of the network trunk cable and the DC ground of the power supply to this ground connection.

DeviceNet standards require a 120 Ohms resistor to be mounted at the beginning and at the end of the line. Robotiq recommends that if the Gripper is at the end of the line, the terminating resistor needs to be connected between pin 4 and 5. You can also take a look at the following figure to have a better idea.

DEVICENET2

The installation of the terminating resistor eliminates the signal reflection effect on the line. In fact, since this effect can damage your devices, it is really important to connect this resistor correctly.

You should note that there is no terminating resistor mounted in the Gripper and that the shield of the cable must be grounded in the robot controller. Make sure to take a look at the Universal Controller User Manual and the accompanying Gripper User Manual on our support page to double check your connections.

DeviceNet References

As I mentioned at the beginning of this article, we do not claim to be communication protocol specialists. So for further information on DeviceNet and related libraries, go to: odva.org 

For further questions or troubleshooting advice, the following links should be helpful:

odva.org

phoenixcontact.com

peigroup.com 

By recognizing the importance of above grounding advice particularly your Gripper should be all set and ready to recognize the DeviceNet communication protocol. Also it is fun to remember that not frying your equipment will make for a much more productive working environment. For further information, go to our support website or give us a call.

Industrial Communication Protocol Cheat Sheet Get it here

Leave a comment

Mathieu Bélanger-Barrette
Mathieu is a production engineer at Robotiq, where he constantly strives to optimize the production line for Robotiq Grippers. He enjoys discovering new robotic applications and sharing what he learns on Robotiq's blog.
Connect with the writer:
http://robotiq.com

Related posts

What's New In Robotics?  14.02.2020

Good morning. In this week's news mix: igus releases new cobot cable management kit, Nissan invests in cobots and 2019 North...

Emmet Cole
By Emmet Cole - February 14, 2020
What the UR16e Means for You and Robotiq

Universal Robots' powerful UR16e is an exciting addition to its product range. But what does it mean for your operations and...

Romy A Letourneau
By Romy A Letourneau - September 23, 2019
Avoid This Common Robot Deployment Mistake This Year

This time of year is when many of us start our new robotics projects. But beware! Don't fall into the trap of over-complicating...

Alex Owen-Hill
By Alex Owen-Hill - January 10, 2019