Subscribe

Latest Blog Post

How Pneumatic End Effectors Work?

Catherine Bernier
by Catherine Bernier. Last updated on Nov 14
Posted on Jun 26, in Automation
3 min read time

neumatic grippers are mechanical devices that are really common in automated manufacturing processes. Combined with a robot they can do many robotic applications such as: pick-and-place, machine tending or assembly. We will talk about how they work generally, including the pros and cons.

Usual pneumatic grippers work using a piston to open and close their fingers/jaws. Air is compressed in the chamber of the piston and, according to the piston size, when it has enough pressure the air will make the piston move. The simple formula to remember is:

Pressure X Surface = Force

Even if these robot grippers all work with the same principle, they may have different configurations:

Angular gripper

The piston in this kind of gripper will make the jaws move around a rotating axis in order to make it close. So it uses a lever to make the fingers move and grasp a part. Here is a picture that explains it all.

angular-gripper-end-effector-Robotiq-pneumatic

In blue, you can see how the air makes the piston move. This type of gripper can provide a fairly large gripping force. However, one gripper can only grip a limited size variation of parts. Other versions of this gripper can include a third or fourth jaw.

Parallel gripper

parallel-gripper-robotiq-end-effector-pneumatic

The next version of pneumatic end effector that we will talk about is the parallel gripper. In this configuration the gripping surface of the jaws remains parallel throughout all their movement. This kind of gripper can also include a third or fourth jaw for gripping unusual parts.

Pros and cons

The pneumatic end effectors are low cost devices that are simple to use and implement. With any type of pneumatic gripper, jaws can be design to fit different kinds of pieces. However, this is also a limitation for this type of device, since it takes different jaws to grip very different pieces. Moreover, using air is another limitation, because as a compressible fluid, the movement of the piston will be less precise, making it very difficult to precisely control force and speed of the jaws.

These are some of the reasons why Robotiq is making electric end effectors. Their movements are more precise since they are made by controllable electric motors. Thus, force and speed of the jaws can be controlled. While pneumatic grippers can only do full stroke (open or close), the electric grippers can do partial closing and opening sequences. Moreover, their adaptive design enables them to grip a large range of different size and shape of parts.

In conclusion, pneumatic grippers are the solution for high volume and low-mix production, because they are simple and low cost. However, the new challenge in the automation industry is about low volume and high-mix production. The best solution for this new need would be electric end effectors. To know which robot gripper is best for you, get our ROI Robot Gripper Calculator.

Related article: How to choose the right Gripper for your application

 DOWNLOAD YOUR  FREE ROBOTIC ROI CALCULATOR

Leave a comment

Catherine Bernier
Written by Catherine Bernier
Catherine is an Application Engineer here at Robotiq. Drawing from her expertise with manufacturing processes, production management and business management in general, her main focus is helping her clients find the solutions that will best serve their needs. If you have any questions about Robotiq's products and how they can serve your application, get in touch with her at c.bernier@robotiq.com.
Connect with the writer:

Related posts

Future-Proofing Production: Lessons from a Leading Meat Processor’s Automation Journey

Robotiq CEO Samuel Bouchard sat down with Josh Davis, senior channel sales manager, to discuss a leading meat producer’s...

Josh Davis
By Josh Davis - January 16, 2025
Automation First Strategy: How to Win in the Future of Work

The landscape of work and business is constantly changing. Every time a new technology or way of working takes its hold on an...

Alex Owen-Hill
By Alex Owen-Hill - December 13, 2022
The Cost of Automation: Do the Numbers Really Add Up?

It's no secret that automation can have a huge impact on the way you do business. But does the cost of automation match the...

Alex Owen-Hill
By Alex Owen-Hill - December 7, 2022