News briefs for the week take a look at new AI-powered robots and cobots for machine tending and logistics operations, mobile UV robots for disinfecting passenger aircraft in 10 minutes, oil rig robot roughnecks entering the drilling industry, the Top 5 picks for countries winning the robotics implementation race for 2021 (and it’s only April!), and the outlook for global industrial robot sales (including peripherals and software) beginning mid-2021.
80 percent of all factory tasks in the U.S. are performed by machine operators, with $650 billion annually spent on machine tending, according to a research article in Control Automation. Currently, there are 600,000 open positions for machine operators, and not
Rapid Robotics (founded in 2019) has built its company at filling that gap with cobot work cells that it calls RMOs or rapid machine operators. “US manufacturers can’t hire machine operators fast enough,” says the U.S.-based company, “and until now they’ve had no viable way to automate the jobs either.”
So, for $25,000 per year, Rapid Robotics will supply one “pretrained robotic machine operator that understands how to perform common machine tasks without programming or systems integration…a complete software and hardware solution that combines proprietary machine vision and deep learning AI with proven robotic hardware to handle most machine operator jobs ‘out of the box.’”
Estimated annual savings per two shifts: $80k.
Another U.S. developer powering robot arms with AI is Ambi Robotics, formerly Ambidextrous Laboratories, co-founded in 2019 by UC Berkeley’s Ken Goldberg. Emerging from stealth mode in March of 2021, with $6 million in seed funding, the company will utilize its AI-powered grasping tech to simplify logistics’ most challenging jobs, like bin picking and automating Put Walls.
The company’s proprietary operating system called AmbiOS, is a spin off Goldberg’s UC Berkeley developed Dexterity Network or Dex-Net, a “first-of-its-kind technology that rapidly trains robots to pick millions of unique items through deep simulation-to-reality transfer learning.”
Dex-Net “trains robots in hours, not months,” claims the company, “10,000x faster than collecting data in the real world.”
The company’s twin AmbiOS software offerings: 1. AmbiSort that sorts for Put Wall shelving from mixed bulk inflow; and 2. AmbiKit, for basic grasping and kitting functions, are, according to the company, “over 50% faster than manual labor.”
For the robot curious: Just three months into 2021, Analytics Insight is out with its picks for which countries are leading the robotics implementation race so far this year (it's only April!).
“The proliferation of robotics has begun well,” opened the report. Here are the five picks. Get the full rundown: Analytics Insight
Robot roughnecks threaten oil rig jobs
The Bureau of Labor Statistics tabs oil rig roughneck as the country’s third most dangerous job, with American and Russian roughnecks the world’s most endangered among their peers. It’s not too hard then to imagine a time in the near future when oil rig work will be totally automated.
“Despite the huge potential of robotics, operators should be aware that these savings will be partially offset by the considerable investments required for the adoption of these solutions, which may vary depending on the cost structure and whether the robots are owned or leased,” says Sumit Yadav, energy service analyst at Rystad Energy.
Nabors claims the automated robotic system operates 40 percent faster and saves $10-$20 million annually.
UVeya claims that its fully automated disinfection robot can be deployed in five minutes and can clean both air and interior surfaces of an aircraft in ten minutes.
Uveya tested the production version of the technology on the aircraft of Swiss regional carrier Helvetic Airways last month, effectively eliminating more than 99% of bacteria and pathogens, including COVID.
Industrial robot sales to spike mid-year
Quince Market Research reports that the Industrial Robotics (with peripherals and software) Market was valued at $51 billion in 2020 and is projected to grow at a CAGR of 10.3% during the forecast period through 2028. Due to the impact of the COVID pandemic, however, the global industrial robotics market valuation has come down $43 billion and is projected to grow at a CAGR of 7.6% during the forecast period.