Blog | Robotiq

Seven robots working for the health of our planet

Written by Philip Fine | Sep 10, 2019 3:33 PM

Machines fueled by trash, super fast recycling sorters, and an invasive species zapper/vacuum: Here are a few of the robotics industry’s environmental ideas for the health of our planet.  

Robots and the environment: a surprisingly healthy relationship. Source: Katarzena Pe

As weather-related disasters appear more frequently and reports on climate change become increasingly urgent, some robotics manufacturers are taking action. These environmental entrepreneurs and researchers are using tech to create alternative energy sources, and to change traditional waste disposal, recycling, and forestry practices. They have also found creative ways to quell the influx of invasive species, diminish e-waste and collect ocean garbage.

Here are seven sustainable robotics initiatives that are giving those inside and outside the tech sector faith in our ability to help clean up some of the mess we’ve made.

Fueling robots with dead flies and rotten fruit

Rotten fruit will help feed microbial food cells. Source: Maria Teneva 

Bristol Robotics Laboratory’s BioEnergy Centre in England has been working on a series of robots that operate on microbial fuel cells (MFCs) MFCs store electrical energy derived from organic matter. While the EcoBot I used sugars as a source of fuel, EcoBot II feeds on a flora of microorganisms from a less appetizing but more sustainable source: dead flies or rotten fruit. Bristol scientists admit that the energy output is far lower than that of traditional batteries, but they see hope for an emerging technology that provides a continuous energy supply for as long as the bacteria can be kept alive.

Electric Mole versus The Sludge

Turning smelly sludge into dry dirt. Source: Thermo-System

Untreated raw sewage not destined for waterways is usually dried. But the drying process takes time, the sludge is difficult to store and the potential for stream-polluting runoff is high. Thermo-System’s Electric Mole, more stripped down autonomous car than animal, does share a feature with the insectivore by being able to displace dirt. It turns and aerates sludge inside a greenhouse-like hall until it turns inert and is no longer smelly. At the end of the drying process, the contents are ready to be transported.

Sorting the recycling at twice the rate

Robots can now sort recycling at super fast speeds. Source: Vivianne Lemay

With China now accepting much less of the West’s recycled materials, several companies have stepped in to recuperate the materials more quickly. The MAX-AI is one of them, identifying and sorting items with the same accuracy as humans but twice as fast.

Yelling “Timber!” under water

Lumberjack of the sea. Source: Treehugger.com

Forestry companies looking to virgin forests for their trees can find many under water. When massive hydroelectric dams are created, huge areas of forest are often flooded. The Sawfish Underwater Harvester, a 7,000 lb, unmanned logging submarine, harvests submerged trees and brings them up to the surface, exploiting an unused resource and saving the all-important above-ground forests.

Invading the space of the invasive species

Vacuuming up an invasive species (RSE)

Lionfish, are an invasive species threatening marine life. The inventor of the Roomba has used that robot and vacuum technology to catch the fish that often invades precious coral reefs. The Guardian, a camera-equipped transparent tank controlled from the surface, allows the operator to identify the fish, get the tank’s paddles up close, zap the fish with electricity and vacuum it into the tank. Operators have been known to provide local cooks with the lionfish, who then serve it up as a local delicacy.

The disassembly line

iPhone in the process of being recycled. Source: apple.com

Apple has found a way to address some of our electronic waste. On Earth Day 2018, they came out with  a system they’re calling Daisy. A successor to Liam, which was debuted in 2016, Daisy removes and sorts components and can take apart up to 200 iPhone devices per hour.

Ocean garbage collector

Gobbling up marine plastic. Source: RanMarine

The Waste Shark, inspired by the whale shark, which swims through water and eats its prey with minimum effort, does the same with plastics, micro-plastics, alien vegetation and floating debris. The remote-control harvester, with its 200-litre capacity, can collect waste, and data, for 16 hours a day.

These are just seven initiatives. Imagine what can be accomplished if more of the world’s robotics manufacturers took up sustainability initiatives. If you’re a robotics maker, will they inspire you to make products that will help solve some environmental problems?