Error - Capability not supported : DIGITAL_OUTPUT_MODE
How to resolve this error by correctly configuring the Tool I/O settings in UR's Installation tab
Context
This article addresses the “Capability not supported : DIGITAL_OUTPUT_MODE” error, commonly encountered when setting up a Robotiq Gripper with a Universal Robots controller. The issue typically results from incorrect configuration in the Installation > Tool I/O section of the UR interface. Proper configuration is essential for the gripper to communicate correctly with the robot.
Error Description
You may see the following error on your teach pendant during setup or when attempting to use the gripper:
This error prevents the gripper from functioning and is caused by an incorrect Tool I/O control setting, depending on your hardware configuration.
Resolution Steps
1. Open Tool I/O Menu
-
On the UR teach pendant, go to Installation > General > Tool I/O Interface.
-
Identify the Control Source setting.
2. Identify Your Coupling Type
Check which type of Robotiq coupling you are using:
-
CB-Series coupling
-
E-Series coupling
-
I/O coupling
3. Apply the Correct Setting
Set the Control Source as follows:
-
CB-Series coupling
→ Set to: Controlled by Users
-
E-Series coupling
→ Set to: Controlled by Robotiq Gripper
-
I/O coupling
→ Set to: Controlled by Robotiq Wrist Connection
⚠️ If you are unsure of your coupling type, refer to this article.
Conclusion
The “Capability not supported : DIGITAL_OUTPUT_MODE” error is resolved by selecting the correct Control Source in the Tool I/O menu, based on your coupling type. Always verify this setting during initial setup to avoid communication issues with your gripper.