Does the Hand-E respect the ISO TS15066 ?
The norme ISO TS15066 is the new norme for the collaborative robot.
Knowledge
For the Hand-E, the specification is :
This information is available on the documentation of the gripper available here.
For the ISO TS15066, there is a recommendation to have the force at a maximum of 140N. But it's only a recommendation and it's not necessary.
So the Hand-E respect the ISO TS15066.