Blog | Robotiq

Meet PAL Ready and PAL Series: Two clear paths to smarter palletizing

Written by Samuel Bouchard | Sep 16, 2025 4:00 AM

Palletizing may look simple—stack boxes, ship them out—but it’s one of the most critical steps in your logistics chain. With 80% of goods worldwide ending up on a pallet, this step is on the critical path between you and your customers. Too often, it’s also where time and money are lost. Many manufacturers only discover the palletizing bottleneck after they automate it, then quickly see operations become more productive, predictable, and competitive.

Manufacturers need palletizing options that deliver results today and scale tomorrow. That’s why at Robotiq we created two clear paths to robotic palletizing:

  • PAL Ready, a production-ready palletizing cell, fully assembled and running on day one.
  • PAL Series, a modular approach that grows with your needs, from one line to multi-site deployments.

Both are powered by the same Robotiq software, tools, and operator experience, so every deployment builds on a proven foundation. And together, they’re part of something bigger: the Lean Palletizing Experience.

At Robotiq, we’ve reimagined what palletizing should be. The result is The Lean Palletizing Experience, a breakthrough in the way manufacturers start and scale automation projects. It’s a complete digital-to-physical journey that transforms automation from complex, custom projects into a productized and scalable solution. 

Two paths to successful automation

PAL Ready

PAL Ready is a production-ready palletizing cell. It is fully assembled, tested, and ready to run on arrival. It helps you automate with confidence, even on your very first cell. PAL Ready includes everything you need and is designed for rapid installs.
 
It comes with a Robotiq Smart Infeed, allowing you to present any box to the palletizer at the right time and at the right place, automatically. It ensures an optimal output of the palletizer with minimum programming intervention. PAL Ready also includes a mobility feature, allowing it to be used on different lines or simply moved out of the way for factory floor cleaning. Safety scanners also come standard with PAL Ready as well as a Robotiq PowerPick Multi Vacuum Gripper.


PAL Series

PAL Series is all about modular palletizing. It’s a configurable option built from our standard models (the AX or PE Series) and modules (Robotiq Vacuum Grippers, Smart Infeed, Safety Packages, and Mobility Kits).  

As your needs grow, you can move from a single unit to multiple units or to modular deployments using the same:

  • Software
  • Building blocks
  • Operator interface
  • Design logic

Either way, there is no need to start over when adding new lines or sites. You grow on a foundation that is already proven. Both paths allow you to start fast and scale with confidence, and they are both part of a bigger picture.

The Lean Palletizing Experience

The Lean Palletizing Experience is more than a new product or two. It is the entire journey from digital entry point to fully functioning, physical platform that is built to scale with your production. Your digital-to-physical journey starts with online validation and design and ends with end-of-line productivity on your factory floor.

Here are the steps:

  1. Select - Find out if your application is a match in minutes with our Palletizing Fit Tool
  2. Simulate - Design and validate your cell layout digitally with our Online Configurator
  3. See - Check out a demo unit in action near you thanks to our Global Partner Network
  4. Start - Launch into production with easy-to-use software, support, and training
  5. Scale - Expand deployments to your other lines to increase your ROI and productivity

You need fast results AND long-term flexibility. The Lean Palletizing Experience by Robotiq resets the standard. It is:

  • Digital-first, so you can validate before you deploy
  • Production-ready, so you can install in under a day
  • Scalable, so you can grow without redesigning
  • Unified, so every site uses the same operator experience

Whether you’re starting with a single cell or planning a multi-site rollout, you stay within the same experience every step of the way.

 

The time to act is now

Automation shouldn’t be a leap of faith. It should be practical, structured, and proven.

The Lean Palletizing Experience, complete with PAL Ready and PAL Series, gives you everything you need to move from manual palletizing to a future-ready solution:

  • Shorter timelines
  • Fewer integration challenges
  • Predictable ROI
  • A safer, more productive workforce

Start fast. Scale with confidence. Embark on your automation journey.
Fill out the Palletizing Fit Tool today and see if PAL Ready or PAL Series is right for your operation.