Why Does the Gripper Work on RUI but Not on a TM/Omron Robot?
Check Modbus settings and COM port configuration when using Robotiq grippers with TM/Omron
Context
Sometimes a gripper works correctly when tested on the Robotiq User Interface (RUI) but fails to communicate with a TM/Omron robot. This article explains the most common cause and how to resolve it.
Information
Main Cause
-
The RUI can control a gripper with any slave ID and baud rate.
-
The TM/Omron robot, by default, can only communicate with a gripper that has slave ID = 9.
How to Fix the Issue
-
Check Modbus RTU Settings in RUI
-
Verify the slave ID of the gripper.
-
If it is not set to 9, update it to match the TM/Omron requirement.
-
Confirm that other communication settings (baud rate, parity, etc.) are at their default values
-
-
Check COM Port Settings
-
Ensure the physical COM port used for the connection matches the COM port defined in the SET node on the TM/Omron robot.
-
1. 
2.

If the Problem Persists
Other causes and solutions may be possible. If the issue is not resolved after checking Modbus settings and COM ports:
Contact : support@robotiq.com