Skip to content
English
  • There are no suggestions because the search field is empty.

What are the different configuration possible for the Screwdriver?

This article is meant to present the dual configuration and various set ups that are possible and good practices.

Generalities

The screwdriver can be used with another Robotiq component, provided that their maximum current consumption is not reached simultaneously (e.g., avoid closing the gripper and reaching the maximum torque at the same time).

Configuration examples

2 Screwdrivers on 45° bracket

 

Screwdriver + Epick on 90° bracket at Automate and Automatica events, here is a link to see it.  


 

Screwdriver + camera +gripper : 

See the video : here

 

See our best practices here.