Skip to content
English
  • There are no suggestions because the search field is empty.

How to Program Rigid Interlayers Using the Multipick Feature 

Learn how to create and configure rigid interlayers, adjust the gripper model, and use a template program in Robotiq’s Palletizer.

To manage interlayers and see it in the interface, you need to : 

       1. Create the “interlayer” box using multipick feature

       2. Configure the interlayer

       3. Replace the automatic gripper model with a custom collision model

You will also find in this article :

       4. Programming concept

       5. Template program link

 

1. Create the " box interlayer" using the multipick features

 

2. how to configure Interlayer: 

optional : 

Contact detection can be used especially if you interlayer is mid soft. It will allow to bring interlayer above the target with an offset :

 - If needed, here is a complete video describing multipick and for more info we recommand using our user manual available on our website.

 

3. Replace the Automatic Gripper Model with a Custom One

 

 

Configure it. X, Y, Z are in the tool referential.

 

4.Understand the Programming Concept

In this example :

 

5. Program template for Rigid interlayers 

here the  link