Skip to content
English
  • There are no suggestions because the search field is empty.

Integrating the Robotiq Palletizer with External Systems

Linking barcode readers, PLCs, and HMIs to the Robotiq Palletizer, and what Robotiq supports

In some production environments, the Robotiq Palletizer needs to interact with external systems. These integrations help improve automation and reduce manual intervention. Typical use cases include barcode validation and rejection, recipe selection from a warehouse or production system, or centralized control via a single HMI. This article explains how such integration can be done, and clarifies what Robotiq supports directly.

Integration Overview

  • Possible? Yes. Our software allows you to add custom logic in the UR program.

  • Supported by Robotiq? Only functionalities available via our Copilot interface and documented APIs. Robotiq does not provide support for external integration setups unless part of an Installation Services project.

Custom integrations must be managed by the integrator or customer, with Robotiq support limited to Copilot functions.

Protocol /Useful Resources from Universal Robot

Useful Copilot Functions (for reference)

EtherNet/IP and PROFINET exception:

Communication through EtherNet/IP and Profinet are possible and require unticking a parameter in the Robotiq URcaps :
  • Go to Installation

  • Select URCaps

  • Open Copilot

  • Untick : “Use Copilot to manage soft speed transition when resuming from a safeguard stop”

  • Save the installation

Related article : 

Example 1: Barcode Reader for Rejecting Boxes

Reject the case if the barcode is unreadable or if the content is flagged for rejection (commonly used in pharma).

What is required:
  • Communication setup with the barcode reader. useful article on UR: using a barcode reader directly with the robot

  • Custom logic in the "Grip" folder:

    • Custom moves to release the box onto a reject conveyor

    • Add the Copilot function rq_ignore_current_box() to skip the palletizing trajectory while keeping the box count unchanged


     
Example 2: Recipe from a PLC/WMS

 

An external system controls which recipe to use, including product status and configurations, without operator input.

What is required:
  • Uncheck the “Validate pallet state at program startup” to skip manual validation

  • Communication setup with external system

  • Use the function rq_set_palletizer_state() to select pallet configuration and start a new pallet

  • Optionally, use rq_set_box_payload() to adapt payload by SKU weight if dimensions remain the same


Example 3 : One HMI for Full Line Control

The entire production line, including the palletizer, is controlled via a single Human-Machine Interface.

What is required:
  • Uncheck “Validate pallet state at program startup” to remove the need for the operator to confirm pallet status

  • Communication with external system

  • Use rq_set_palletizer_state() before starting a new pallet to select the recipe and status

  • Optionally, use rq_set_light_state() to match the tower light signal to the other equipment on the line (e.g. upstream fault)


Conclusion

Integrating the Robotiq Palletizer with a barcode reader, a PLC or WMS, or a line HMI is done by adding your own logic to the UR program and calling the public Copilot functions. Robotiq supports the Copilot functions and the documented APIs; the custom integration itself stays with the integrator or the customer, unless it is part of an Installation Services project.

Need help? Contact Robotiq Support.

Updated: spetember 21 , 2026