How to control an I/O coupling on other robots ?
Wiring, signal types, and preset control using the I/O Coupling on robots not natively supported by Robotiq
Context
The I/O Coupling allows you to control Robotiq adaptive and vacuum grippers using just two digital inputs and two digital outputs from your robot. These I/Os are used to trigger preset actions that are preloaded into the gripper.
For supported robots like Universal Robots (CB3 series), Techman, and Omron/TM, we provide dedicated software components to manage these I/Os automatically.
However, in custom applications—such as integrating with a robot that has digital I/Os but is not supported by our software—you can program your own I/O logic to trigger these presets manually.
Prerequisites
To use the I/O Coupling with your robot, you’ll need:
-
A Robotiq gripper
-
A Robotiq I/O Coupling module (UR or TM variant)
-
A robot with:
-
At least 2 configurable digital outputs
-
At least 2 digital inputs for feedback
-
Matching signal type (PNP or NPN) with the I/O Coupling variant
-
-
A power supply connected through the wrist cable or equivalent
⚠️ Important: Using the wrong I/O type (e.g., PNP vs NPN mismatch) may prevent operation or cause hardware damage.
Electrical Compatibility
The Robotiq I/O Coupling comes in two variants:
| Variant | Compatible Robots | IO Type |
|---|---|---|
| UR version | Universal Robots (CB3 series) | NPN outputs, PNP inputs |
| TM version | Techman and Omron/TM robots | PNP outputs, NPN inputs |
What's PNP vs NPN?
-
PNP (sourcing output): sends positive voltage to the load
-
NPN (sinking output): connects load to ground
Your robot’s digital outputs must match the I/O Coupling’s inputs, and vice versa.
❗ Example: Doosan use PNP for both input and output so TM or UR IO coupling cannot be used by connecting it to the wrist.
Pin Mapping and Connections
The I/O Coupling uses a 4-pin connector. Here is the pinout:
| Pin | Function | Direction | Description |
|---|---|---|---|
| 1 | Input A | From robot | Digital signal A (preset selection) |
| 2 | Input B | From robot | Digital signal B (preset selection) |
| 3 | Output A | To robot | Gripper status |
| 4 | Output B | To robot | Gripper status |
Make sure the wiring respects signal levels and polarity based on your robot’s I/O type.
Activation of the I/O Coupling
To get the I/O Coupling working in a custom setup, you’ll need to perform an initialization (activation) step before using the presets.
Use the two connected robot output lines (the two I/O inputs to the coupling) to send an initialization command to the gripper. This allows the coupling/gripper to calibrate its positions. Without this step, the gripper won’t properly “activate,” and presets may not behave as expected.

Controlling Presets with I/O
The I/O Coupling interprets combinations of signals on Input A and B to trigger predefined gripper actions. These actions (presets) are stored in the gripper’s memory.
Command Signals
| Input A | Input B | Triggered Preset |
|---|---|---|
| 0 | 0 | Preset 0 |
| 0 | 1 | Preset 1 |
| 1 | 0 | Preset 2 |
| 1 | 1 | Preset 3 |
Reading Gripper Status
The I/O Coupling sends back feedback via Output A and B. The meaning of each signal combination is:
| Output A | Output B | Gripper Status |
|---|---|---|
| 0 | 0 | Not ready |
| 0 | 1 | Ready for command |
| 1 | 0 | Object detected |
| 1 | 1 | Command in progress |
Use your robot’s digital input monitoring to track these outputs.
Conclusion
The Robotiq I/O Coupling provides a flexible way to integrate Robotiq grippers with any robot platform that supports digital I/O. By sending simple 2-bit signals, you can trigger multiple gripper presets and read status information—no software integration required.