Skip to content
English
  • There are no suggestions because the search field is empty.

Programming Soft Interlayers with Custom Moves

This article aims to show the method to perform soft interlayers requiring custom moves. This method add benefits to the end user : -Flexibility to reprogram -Visible in the user interface when starting a program.

Application example : 

https://share.robotiq.com/public/softintervideo

Here conditions required to be able to program : 

  • Step 1 : Create an Interlayer Box Type

    • Use the Multipick feature to define an item called Interlayer in your pattern.

    • This will let you reference it like a box, but use custom behavior.
  • Step 2 :Use a Custom Gripper Model

    • Replace the default automatic gripper model with a smaller or simplified model.

    • This allows easier handling of thin or flexible interlayers and avoids interference.

Those steps are detailed further if needed.

Scripts documentation

We will use script function available to perform example.All script documentation can be found on the pdf attached when you download our Urcaps. for example a usefull fonction to get pallet height to perform your custom moves : 

rq_pal_get_current_height()M,U: Get the cumulative height from floor of
the current layer.

Program concept : 

  • Use a string variable like boxtype, initialized in the "Before Start" section : boxtype=""
  • Use a conditional block that checks if the current box type is Interlayer
  • If the box is an interlayer, skip the normal palletizing node to avoid applying the default trajectory thanks to script command :rq_ignore_current_box()
  • Manually insert the moves required to place the interlayer at the desired location on the pallet.
  • After placing the interlayer, proceed with the next box in the sequence using the script rq_set_palletizer_state()

Example : 

This example does not work for interlayer as a last box to be placed to perform it see "advanced example" section

image-Apr-04-2025-10-50-23-5261-AM

Conclusion
By combining a custom “interlayer” box, gripper adjustment, and conditional logic, you can integrate soft interlayers cleanly into your palletizing program. This method improves flexibility and makes the interlayer behavior visible to operators.


Advanced example allowing to manage interlayers on top of a pallet and left /right pallet moves : 

 

2026-05-22_11-48-17

Program Model to download : Link

Detailled step 1 and 2 :

1. Create the " box interlayer" using multipick

 

2; - Replace the automatic gripper model with custom model