Skip to content
English
  • There are no suggestions because the search field is empty.

How to Perform Preventive Maintenance on the Hand-E Gripper

Step-by-step maintenance procedure using the Maintenance Kit

Context

This article explains how to perform preventive maintenance on the Robotiq Hand-E gripper using the HND-MAINTENANCE-KIT. Maintenance should be done every 2 million cycles to ensure optimal performance, durability, and cleanliness of internal components.

 

Information

1. When to Perform Maintenance

  • Perform maintenance every 2 million cycles.

  • Signs of need may include inconsistent motion, debris buildup, or reduced grip performance.

2. Tools and Kit Required

  • HND-MAINTENANCE-KIT

  • 4 mm hex key

  • Degreaser

  • Dry towels

  • Safety gloves and eyewear

 

3. Maintenance Procedure

  1. Position the Gripper

    • Open the gripper to an intermediate position to ensure the six M4 screws on the rack housing are accessible.



  2. Detach the Gripper from the Coupling

    • Use a 4 mm hex key to remove the four (4) M5-0.8 x 25mm screws.

    • Each screw includes a tooth lock washer—make sure not to lose them.

  3. Remove the Rack Housing

    • Unscrew the six (6) M4 screws that hold the rack housing in place.

    • Carefully pull the rack housing away from the gripper body.

  4. Extract and Clean Moving Parts

    • The two finger racks will slide off freely.

    • Clean the following with degreaser, then dry thoroughly:

      • Rack housing

      • Finger racks

      • Pinion

    • Use a dry towel to clean:

      • Finger holders

      • Fingertips

      • Coupling (especially the electrical contact area)




  5. Replace Damaged Racks or Pinions (if necessary)

    • Inspect the racks and pinion for:

      • Broken or chipped teeth

      • Uneven wear

      • Rust or corrosion

    • If damage is found:

      • Replace the component using the spare parts included in the HND-MAINTENANCE-KIT

      • Follow the same reassembly steps after replacement

  6. Greasing the Racks

    • Apply grease on all surfaces of the racks except the face with the tapped holes.

    • Ensure even coverage and no excess grease on contact surfaces.

     

  7. Final Inspection and Reassembly

    • Visually confirm:

      • All cleaned areas are free of debris

      • Electrical contact is clear

      • No visible damage

    • Reassemble all components in reverse order:

      • Reinsert finger racks into rack housing

      • Reattach housing to the gripper body

      • Secure the gripper to the coupling using the M5 screws and washers




Conclusion

Performing regular maintenance on the Hand-E gripper extends its life, ensures safe operation, and maintains precise performance. Always follow the recommended 2-million-cycle schedule and use the official HND-MAINTENANCE-KIT.

Watch the full video tutorial: Hand-E Maintenance Video

 

 

Updated

December 2025