Skip to content
English
  • There are no suggestions because the search field is empty.

Installing and Uninstalling a URCap in Universal Robots

A step-by-step guide for properly adding or removing a URCap.

This article explains how to install or uninstall a URCap on a Universal Robots (UR) robot. A URCap is a software plugin that adds specific functionality to your robot, such as hardware integration or new commands.

Important: Some URCaps are downloaded as ZIP folders containing multiple files. To ensure successful installation, you must extract the .urcap file before copying it to your USB drive. The robot will not recognize a zipped folder.

Information

✅ 1. Download the URCap

✅ 2. Check if the file is zipped

  • Locate the downloaded file on your computer.

  • If it is a .zip folder, extract the contents first.

  • Inside, you will see the actual .urcap file and possibly other files (like Release Notes).

  • Only copy the .urcap file to your USB drive.

✅ 3. Copy the .urcap file to a USB drive

  • Use a USB drive formatted to FAT32, if possible.

✅ 4. Insert the USB drive into the UR controller

  • Plug the USB stick into the robot’s teach pendant or controller.

✅ 5. Install the URCap in Polyscope

For CB-Series robots:

  • On the robot’s teach pendant, open the Setup Robot tab.

  • Navigate to URCaps Setup.

  • Click + Add URCap and select the .urcap file from your USB drive.

  • Restart Polyscope if prompted.

For e-Series robots:

  • On the teach pendant, tap the hamburger menu (☰) in the top-right corner.

  • Go to Settings > System > URCaps.

  • Tap + Add URCap and select the .urcap file from your USB drive.

  • Restart Polyscope if prompted.

✅ 6. How to uninstall a URCap

For CB-Series robots:

  • Open Setup Robot > URCaps > Manage URCaps.

  • Select the URCap you want to remove.

  • Click - Remove URCap.

  • Restart Polyscope if needed.

For e-Series robots:

  • Tap the hamburger menu (☰) in the top-right corner.

  • Navigate to Settings > System > URCaps.

  • Tap the URCap you want to remove.

  • Tap - Remove URCap.

  • Restart Polyscope if needed.

Conclusion

Extracting the .urcap file before installation helps avoid errors. Always follow the correct path in Polyscope for your robot series (CB or e-Series) to ensure proper installation or removal.

 Need help?  contact Robotiq Support.

Updated

July 2026