Skip to content
English
  • There are no suggestions because the search field is empty.

Configuring the Box Sensor Input in Robotiq’s Palletizing Workcell

Learn how to connect and configure a box detection sensor using a digital input

Context
This article explains how to connect and configure a box sensor in the Robotiq Palletizing Workcell. This sensor detects box presence on the conveyor and helps trigger pick actions.

Information

1. Connect the Sensor to the Controller

  • Wire the box sensor to a digital input on the controller, such as DI4.

  • Make sure the wiring follows the sensor’s power and signal requirements

 

Box sensor connections

2. Rename the Digital Input for Clarity

  • On the robot’s Installation tab, locate the digital inputs.

  • Rename the DI you used to something clear, such as box_sensor.

rename_box_sensor

3. Select the Box Sensor Input in the Palletizing Node

  • Go to the Palletizer node in your program.

  • Open the Settings menu.

  • In the Box presence input dropdown, select the renamed DI (e.g., box_sensor).

 

Palletizer node Settings tile, with the Edit button circled.

select_box_sensor_input

4. (Optional) Add a Delay Between Detections

If your box sensor is positioned slightly upstream from the conveyor end stop, you can add a delay to better time the detection.

  • Still in the Settings menu, scroll to the delay option.

  • Set the delay time to match your conveyor and box spacing.


add_delay_between_box_detection

Conclusion
Your box sensor input is now fully configured. It will help the Palletizing Workcell detect incoming boxes and trigger pick sequences at the right moment. Need help? Contact Robotiq Support.

Updated: July 15, 2025