Skip to content
English
  • There are no suggestions because the search field is empty.

Differentiating a UR CB3.0 Controller from a UR CB3.1 Controller

Identify the controller version to avoid URCap compatibility issues

Most Robotiq URCaps are compatible only with the CB3.1 controller. If a product fails to work after a URCap update on a UR CB-Series robot, it's important to verify which controller version you’re using. Here are two methods to help you identify whether your robot uses a CB3.0 or CB3.1 controller.

Information

Method 1: Check the Polyscope Installation Medium

Ask yourself: "Is Polyscope installed on a flash card or a USB drive?"

  • If Polyscope is installed on a compact flash card, the robot is using a CB3.0 controller.

CB3.0 systems use compact flash memory cards for Polyscope

Compact flash memory card used by a UR CB3.0 controller to store Polyscope


  • If Polyscope is installed on a USB drive, the robot is using a CB3.1 controller.

     

CB3.1 systems use USB sticks instead of flash cards.

USB drive used by a UR CB3.1 controller to store Polyscope

 

Method 2: Use the Robot Serial Number

If you can’t check the controller directly, use the robot's serial number to determine the version.

Robot From To
UR5 2014350001 2016351863
UR10 2014300001 2016301178

If your robot’s serial number is higher than the listed range, it likely uses a CB3.1 controller.

 

Conclusion

Knowing whether you’re working with a CB3.0 or CB3.1 controller helps ensure compatibility with Robotiq URCaps. Check the memory type or serial number to confirm your controller version and avoid unexpected issues. Need help? Contact Robotiq Support.

Updated: August 14, 2026