Camera Calibration in Confined Spaces
How to calibrate your Robotiq Wrist Camera in tight environments using a two-step method with full calibration and a new local workplane.
Context
If your workspace is too cramped for proper camera calibration, don’t worry—you can still achieve accurate results. Perform a full calibration in an open area, then relocate the robot to the confined space and define a new workplane and camera position, without repeating the full calibration process.
Information
1. Step 1: Execute Full Calibration in an Open Space
-
Start by calibrating the camera in an area with sufficient room for movement.
-
Use Full Calibration in the Wrist Camera setup—this establishes the necessary camera-to-workplane mapping

Step 2: Reuse Calibration in a Confined Area
-
Move the robot to the restricted workspace.
-
Create a New WorkPlane and Position, and define the camera’s Snapshot Position within this environment.
-
Since the full calibration parameters are already applied, you don't need to physically move the robot around the snapshot position again.
-
This setup lets the camera operate correctly even when direct movement is limited.

Visual Support
-
A short video tutorial is available on Robotiq’s eLearning platform to guide you through the process.
You can have a look at this video to help you: Link