Guidelines for Managing Protective Stops on Robotiq Palletizing Solutions
Best practices to reduce false P-Stops caused by payload shifts, vibrations, or grip inconsistencies
Context
Protective stops (P-Stops) can occur during palletizing operations when the robot detects unexpected forces or collisions. These events are often triggered by factors such as payload changes, unstable box gripping, or sudden robot accelerations. This article outlines proven methods to reduce or eliminate false P-Stops when using Robotiq’s Palletizing Solution (PAL).
Robot Motion & Payload Management
-
Reduce acceleration and speed
Preferred strategy when the cycle time allows it.-
Reduces strain on the robot and lowers vibration, especially when the vertical axis (AX) is at its highest.
-
-
Manual payload change
Use manualset_target_payload()commands rather than relying solely on the PAL URCap.-
Example:
set_target_payload(new_payload, new_cog)
-
-
Wait is_steady before and after payload change
-
Add
wait_is_steady()before updating the payload to avoid applying force mid-trajectory. -
Also use
wait_is_steady()after setting the new payload to allow vibrations to settle.
-
-
MoveL at low acceleration after grip
-
Insert a short
moveLjust after gripping the box. -
Use very low acceleration to control the initial motion and reduce residual forces from the suction.
-
Set
target_payloadjust after vacuum ON.
-
Box & Grip Quality
-
Use new, undamaged boxes
Deformed boxes reduce suction reliability and may slip, triggering a P-Stop. -
Test with a lighter box
Helps determine if the P-Stop is caused by the payload weight or other factors. -
Modify suction cup position on the box
Teach the pick position with cups as far apart as possible.-
A wider grip reduces sway and vibration.
-
-
Modify the pick position to increase vacuum cup compression
Adjust the height to create more or less compression depending on your setup.-
Helps avoid box movement during grip.
-
Vacuum and Gripper Behavior
-
Check pneumatic pressure
A weak vacuum results in poor grip and increases risk of dropping the box. -
Use
wait_is_steady()before gripper release
Ensures the robot is stationary before releasing the box, which helps prevent unwanted force feedback. -
Set a higher drop position than the actual pallet
In the PAL node, teach a drop height slightly higher than the physical surface.-
Prevents contact before the box is fully released.
-
Especially useful when using blow-off, which can apply upward force.
-
-
Release with incremental payload change
Allows a smoother transition when updating the payload after drop-off.-
Helps avoid a sudden jerk that can trigger a stop.
-
URCap Parameters & Safety Settings
-
Set safety mode to "Least restricted"
Within installation settings, select “Least restricted” mode.-
Makes the robot less sensitive to minor external forces.
-
-
Use
find_surfacebefore gripping
Compresses the suction cup without robot movement when vacuum turns on.-
Reduces impact forces on the robot during grip activation.
-
-
Activate freedrive before gripping
Temporarily enable freedrive mode before vacuum ON.-
For example:
freedrive([0,0,1,0,0,0])allows motion only on Z-axis. -
Helps absorb vertical shift during grip activation.
-
Additional Tips
-
Adjust pick position to reflect TCP and CoG
Make sure the taught pick position reflects the actual Center of Gravity.-
When CoG is far from the flange, it increases the pendulum effect.
-
-
Ensure TCP and payload values are accurate
Incorrect payload or CoG settings lead to poor motion control.
Conclusion
Reducing false Protective Stops in palletizing requires careful tuning of motion parameters, payload management, and grip quality. The strategies above can be tested and combined based on your application’s constraints. Always validate each change one at a time to isolate the root cause of the issue.