Skip to content
English
  • There are no suggestions because the search field is empty.

Digital Inputs from Screw Feeder Not Showing Correctly

The digital inputs sent by the screw-feeder is not showing up in the URCap on the Teach Pendant.

roubleshooting

1. Check Each Connection in the Circuit

Screw Feeder
  • Use a multimeter to verify that 24 V is present on both output pins at the back of the feeder.

  • To measure voltage:

    • Place one probe on either READY or STATUS pin.

    • Place the other probe on GND.

If you don’t measure 24 V, there may be an internal wiring issue inside the screw feeder.

 

Controller
  • Check that the wires connecting the screw feeder to the robot controller are:

    • Properly screwed in

    • Connected to the correct input slots

  • If any wires are loose or misaligned, reposition and secure them firmly to ensure proper signal transmission.

Robot Installation
  • Open the I/O tab on the robot interface.

  • Observe the Digital Inputs while:

    • Turning the screw feeder ON and OFF

    • Detecting a screw

Manual Test
  • To manually test an input:

    • Use a small wire to connect a 24 V slot to the Digital Input (DI) slot you want to verify.

    • This simulates a signal and helps confirm if the robot is receiving it.

  • If the input still does not respond, try a different DI slot on the controller.

URCap
  • In your program, open the Pick_Screw node.

  • Verify that the correct Digital Input is selected from the drop-down menu.

  • If needed, test other available inputs to determine which one corresponds to the signal from the screw feeder.

 

PNP / NPN Configuration
  • Ensure the system is set to the correct PNP or NPN mode, depending on your wiring.

In PNP mode (reverse logic for NPN):
  • IO Screw Ready:
    → 24 V when a screw is ready
    → 0 V otherwise

  • IO Status:
    → 24 V when the feeder is running properly
    → 0 V if there is a fault

 

 

Info:
For Universal Robots, the switch should be toggled to PNP (towards the rail knob).