Skip to content
English
  • There are no suggestions because the search field is empty.

Controlling ActiveDrive through TCP/IP Communication

Send commands and receive real-time state feedback from the ActiveDrive feature over Ethernet

The ActiveDrive function in Robotiq’s URCap lets users manually guide the robot (force-guided programming) or activate contact-based motion. In some setups, it can be useful to remotely control ActiveDrive modes and stream its internal state via TCP/IP, using a separate device like a PC or PLC.

This article explains:

  • What commands are available over TCP/IP

  • What kind of data can be streamed

  • How to use the communication port

  • Best practices and troubleshooting tips

Knowledge

Overview of Commands to use ActiveDrive via the TCP/IP Socket

Here are the available commands to use the ActiveDrive mode via the TCP/IP socket.

Port 63355

ActiveDrive States

ActiveDrive has different states. To return the current ActiveDrive state, use the GET STATE command. Two states are considered active while the others are transient.

Here are the possible states:

Active:

  • READY → ActiveDrive is ready to run
  • ACTIVE → ActiveDrive is running

Transient:

  • ON_INI
  • ON_READY
  • ON_START_RTDE
  • WAITING_FOR_RTDE
  • WAITING_FOR_ACCEPTABLE_WRENCH
  • WAITING_FOR_ROBOT_PROGRAM

ActiveDrive Settings

Here are the commands to configure the ActiveDrive settings:

  • SET KINETIQ ON/OFF → Kinetiq ON allows the user to move the robot according to the selected options.
  • SET ZERO → Resets the force values applied on the sensor.
  • SET MODE TRANSLATION / FREE / PLANE / SCARA / DOMINANTAXIS 
    • TRANSLATION  (X,Y,Z)
    • FREE (X,Y,Z,RX,RY,RZ)
    • PLANE (X,Y)
    • SCARA (X,Y,Z,RZ)
    • DOMINANTAXIS (X, Y, or Z, depending which force is greater)
  • SET REORIENTATION ON/OFF → Reorientation ON will snap TCP onto the closest orthogonal base frame.
  • SET CONTACT ON/OFF → 
    • Contact ON: For low speeds, when tool is in contact with a surface, for precise movement, for insertions
    • Contact OFF: For high speeds, movement in space

Testing the Commands

Here are the responses you will receive for each command sent:

Command Response
GET STATE GATE STATE XXX
SET KINETIQ XXX SET KINETIQ XXX DONE
or
ZERO ERROR KINETIQ START
if too much force was applied on the sensor to start ActiveDrive
SET ZERO SET ZERO DONE
SET MODE XXX SET MODE XXX DONE
SET CONTACT XXX SET CONTACT XXX DONE

PORT 63356

To display the state of ActiveDrive in real time, open port 63356. It will stream the state at a rate of 62.5Hz (16ms).

...

{"INIT_STAGE": X, "STATE": X, "CONTACT": X, "MODE": X, "REORIENTATION": X, "VISIBLE": X, "PROTECTED": X}

{"INIT_STAGE": X, "STATE": X, "CONTACT": X, "MODE": X, "REORIENTATION": X, "VISIBLE": X, "PROTECTED": X}

{"INIT_STAGE": X, "STATE": X, "CONTACT": X, "MODE": X, "REORIENTATION": X, "VISIBLE": X, "PROTECTED": X}

...

INIT_STAGE

0 primaryClientError
1 rtdeClientError
2 notLicensedError
3 sensorError
4 robotNotRunningError
5 programRunningError
6 targetSpeedFractionError
7 teachButtonPressedError
8 noError
9 finalErrorEnum

 

STATE

0 ON_INIT
1 ON_READY
2 READY
3 ON_START_RTDE
4 WAITING_FOR_RTDE
5 WAITING_FOR_ACCEPTABLE_WRENCH
6 WAITING_FOR_ROBOT_PROGRAM
7 ACTIVE

 

CONTACT

0 No contact / high speed
1 On contact / low speed

 

MODE

0 FREE        (X,Y,Z,RX,RY,RZ)
1 TRANSLATION       (X,Y,Z)
2 ROTATION       (RX,RY,RZ)
3 SCARA       (X,Y,Z,RZ)
4 PLAN       (X,Y)
5 DOMINANTAXIS (X,Y,Z)

 

REORIENT

0 Re-orientation ON
1 Re-orientation Off

 

VISIBLE

0 Toolbar visible
1 Toolbar hiden

 

PROTECTED

Indicates if the ActiveDrive binary is encrypted. Default value is “Protected.” An FT 300-S Force Torque Sensor or a Copilot licence is therefore necessary to run ActiveDrive.

0 Unprotected
1 Protected

Here is the procedure in PDF to help you : Link here

 

Conclusion

Robotiq’s ActiveDrive feature can be controlled and monitored remotely via TCP/IP using a simple command and streaming interface. This is ideal for advanced automation, hands-free setup, or integration with external systems.

Need help? Contact Robotiq Support