Skip to content
English
  • There are no suggestions because the search field is empty.

**Deprecated** Changing the Real-time Ethernet Communication Protocol of a Robotiq Universal Controller

Switch a Universal Controller between EtherCAT, Ethernet/IP, Modbus TCP and ProfiNET.

It is possible to change the communication protocol of a Universal Controller.

  • EtherCAT
  • Ethernet/IP
  • Modbus TCP
  • ProfiNET

The procedure is indicated in the following document: Link

The software NetIC can be downloaded here :  NetIC

 

However, this procedure will not work for those communication protocols:

  • CANopen
  • DeviceNet

No procedures exist as of now to change these communication protocols.

Need help? Contact Robotiq Support.

Updated: October 15, 2026