What are the recommandation for the Air supply setup ?
To ensure good performance and reliability, the Screwdriving solution need a proper air supply. Here is an example of such setup.
1. Air supply requirements
The air supply must be dried and filtered according to ISO 8573-1 class 3.4.3.
An air dryer is required on the line.
For the Screwdriving solution air supply pressure should be set between 6.2 bar and 7 bar (90 psi and 100 psi) at the tool with an optimal pressure set at 7 bar (100 psi).
2. Proper setup example