What is Kaizen? How can you apply it to robotics? This handy check list makes sure you don't miss anything.
Kaizen is one of the main pillars of Lean Manufacturing and, by extension, of Lean Robotics too. It means "continual improvement" and the word comes from the Japanese (改善) meaning "change for the better" or simply "improvement." It does not refer to a specific business technique — it is more of a mindset which can be developed by using a set of techniques.
The kaizen approach is to create a culture of improvement within your business. Rather than imposing changes from the top down, it encourages collaborative improvement from everyone on the team every day.
Use the following list to move forward with your implementation of kaizen in your robot deployment process. Copy it and circle or fill in your chosen options.
|
Which Kaizen Will You Focus On? |
Flow kaizen |
Process kaizen |
||
|
Which Concepts Do You Still Need to Learn? |
PDCA |
5S |
5 Whys |
The 10 Wastes |
|
Kaizen Event, Daily Kaizen or Both? |
Kaizen Event |
Daily Kaizen (highly recommended) |
||
|
How often will the team hold kaizen meetings? |
Every |
days |
||
|
Have You Got the Lean Robotics Book? |
Yes |
Not Yet (get it here!) |
Kaizen affects the entire business. However, there are two different levels of kaizen. Although both should include team members from every level of the business, each requires a slightly different approach. Make sure that you know which you are tackling before you begin.
The two levels of kaizen:
It is common to begin by implementing low-level, process kaizen by organizing a "Kaizen Event" (which I describe below). This is quick, cheap and effectively teaches kaizen concepts to the team using a specific, clear example. After this is successful, you can then move on to introduce flow kaizen to your over business.
Lean Robotics is based on several different techniques, which you can read about at leanrobotics.org. Kaizen utilizes many of these to achieve continuous improvement. It's helpful to familiarize yourself with these techniques before you start to implement Lean Robotics in your business.
Some of the most important techniques for kaizen are:
The goal of kaizen is to achieve small but significant changes every day. This is often referred to as "Daily Kaizen." For this to be effective, you should hold regular team meetings to reinforce the improvements that have already been implemented and seek new ones.
You should decide:
As well as Daily Kaizen, it can also be beneficial to organize a one-off Kaizen Event (aka Kaizen Blitz), where the whole team works together for a day to improve a particular aspect of one individual process. This can be a good opportunity to teach your team about kaizen and experience its effect immediately with your robot cell.
If you are running a Kaizen Event for your robot deployment, here are some questions you might consider:
When the event arrives, the team should work together to improve the process using whichever metric is most relevant to measure the results.
It is highly recommended to include Daily Kaizen into your regular schedule. Although Kaizen Events can be a great way to see instant changes, they are not so effective when used in isolation as they do not maintain the improvements.
Kaizen is only one of the many aspects of Lean Robotics which can help to make your robot deployment a success.
If you haven't yet got your free copy of the Lean Robotics book, make sure to get it by visiting leanrobotics.org!