By looking at the machine runtime you will be able to see how to get the most out of your machines.
While talking with people in many different industries I realized a common approach that people instinctively fall back on when looking at automation. The first thing that comes to mind when you are overloaded with production is to add another machine. This seems to be the simple and fastest way to keep up with production. However it also has some other repercussions.
You may need to hire another employee, you will have to do maintenance on that machine as well and most of the time, when you buy a new machine it contains added
Having the machine run for extra unattended hours has some nice positive impacts that you may not be able to get if you decide to buy a new machine instead. For example, in a CNC shop, most of the time your selling price will be related to the spindle time you need to produce that part plus some added value tasks that need to be done on each part (deburring, coating and so on). So having the machine run extra hours, you get more spindle time per day which implies more selling power per day! Furthermore, employees can be monitoring the robotized loading process while deburring or doing other value added tasks. This way, the time spent deburring or doing other processes to the part is added in a parallel manner to the machine spindle time, whereas it used to be done in a series to this process. Because traditionally the employee had to feed the machine and wait until it was done before moving on to other tasks.
When looking at automating various tasks, again my tip is that you should get advice from automation and robotic experts when you get to this point. They are constantly involved with new technologies and they know what is available that can help you out.
Read more about optimizing productivity in our eBook: Optimizing the Productivity of Existing Equipment.