Medra Lab 001 is the largest autonomous AI-driven laboratory in the United States, operating continuously with robotics, AI, and adaptive grippers.
Medra Lab 001 never sleeps. It reads the literature, designs experiments, runs them, analyses the results, and decides what to try next — continuously, without a human at the bench.
Built across 38,000 square feet in under 90 days, it is already running in production with partners including Genentech.
This is Physical AI in its clearest form: software intelligence closing the loop on physical action, at scale, 24/7.
Despite two decades of lab automation, only ~5% of lab instruments are automated.
Medra’s answer is a Vision-Language-Lab-Action model, capable of operating more than 75% of existing lab instruments.
This system can:
Applications already include:
Medra Lab 001 is a production-scale autonomous lab, with:
This matters because Physical AI systems depend on large volumes of consistent physical data, which is something most labs still cannot generate reliably.
In automated biology labs, robots must handle objects designed for human hands:
This creates a core challenge:
Variability is constant.
Fixed tooling fails as soon as workflows change. And in high-throughput labs running hundreds of protocols, change is the norm—not the exception.
Medra selected the Robotiq 2F-140 Adaptive Gripper across its robotic fleet.
This gripper enables:
At fleet scale, this delivers a critical outcome:
Robots can operate continuously, without manual intervention or reconfiguration.
For Physical AI systems, hardware decisions directly impact AI performance.
Using standardized end-of-arm tooling across all robots:
This is a data strategy.
Medra’s system highlights three principles for building scalable Physical AI platforms:
At scale, downtime limits how much useful data your system can generate.
Hardware rated for millions of cycles becomes core infrastructure.
Identical tooling across robots improves data consistency and reduces operational complexity.
Grippers that handle variability mechanically reduce the burden on AI models—especially in high-mix environments.
AI can design the experiments.
Execution is still physical.
And in systems like Medra’s, the hardware at the end of the robot’s arm is what separates:
Evaluating end-of-arm tooling for a Physical AI or lab automation application?
Whether you're:
Talk to a Robotiq expert to get practical recommendations for your application.