Blog | Robotiq

Debunking the “20-pound rule”: Why weight isn’t the only risk in manual lifting

Written by Samuel Bouchard | Jun 10, 2025 7:11 PM

"Is it under 20 pounds? Then it’s fine to lift."
 That myth has lived too long on factory floors.

In reality, the dangers of manual palletizing aren’t just about how much your team lifts—but how often, how far, and how awkwardly. The so-called “20-pound rule” overlooks the cumulative toll of repetitive motion, poor posture, and non-stop shifts. And for food and beverage manufacturers, that can mean rising injury risks hiding in plain sight.

Let’s unpack why weight alone is a misleading metric—and what to focus on instead.

What the "20-pound" rule gets wrong

At first glance, 20 pounds doesn’t sound like much. But lift that same box 600 times a shift? That’s 6 tons of total weight moved in a day—often with twisting, reaching, and bending mixed in. The strain builds fast, especially when the pace is relentless.

Here’s what weight-only thinking ignores:

  • Repetition: Even light loads, done frequently, lead to muscle fatigue and joint stress.
  • Posture: Awkward lifts from below the waist or above the shoulders dramatically increase the chance of back and shoulder injuries.
  • Distance: Lifting boxes farther from the body increases the force required—and the risk.
  • Speed and pressure: Palletizing is a time-sensitive task. That pressure adds tension and risk to every movement.

That’s why ergonomic experts—and safety agencies like NIOSH—use more holistic tools to evaluate lifting risk.

 

What actually matters: The real risk factors 

Tools like the NIOSH Composite Lifting Index (CLI) account for:

  • Frequency and duration of lifts
  • Vertical and horizontal reach distances
  • Twisting and asymmetry
  • Coupling (grip quality)
  • Load weight and handling zone

A CLI score above 1.0 means elevated risk. Over 3.0? You’re likely on borrowed time before someone gets hurt.

Spoiler alert: Many manual palletizing tasks hit that threshold fast—even when boxes weigh less than 20 pounds.

 

The cost of ignoring ergonomic reality 

Injury from overexertion isn’t just painful. It’s expensive:

  • $39,000+ average cost per back injury
  • Weeks of downtime and lost output
  • Higher turnover, harder recruiting
  • Increased insurance premiums

And the worst part? These are preventable.


What to do instead: Eliminate the lift, not just the weight

The best way to protect your people (and your margins)? Get them out of the danger zone entirely.

Robotic palletizing with a Robotiq cobot system means:

  • No more repetitive lifting
  • No more awkward postures
  • A CLI score of zero

  • And a system that installs in just 3 days, with no facility redesign

In other words: Less risk, more reliability—and a workforce that can focus on higher-value work instead of repetitive strain.

 

Bottom Line: Don't let a number fool you

That 20-pound box might seem harmless. But the truth is, weight is just one piece of the puzzle. If you’re still relying on outdated rules of thumb, you might already be risking more than you realize..

💻  Join our ergonomics webinar with certified safety expert Carla Silver - register today!

📘 Need more details and statistics? Download our Ergonomics ebook, also by Carla Silver.