The 6th edition of the trade show Automatica, held in Munich, Germany, is the spot to be if you are in the robotic, mechatronic or automation business. The show is in a couple of days. It starts June 3rd and continues on until the 6th. Several companies are anticipating this show as they will be launching new products or showing major upgrades to their existing technologies. Since this show is huge and there are a lot of exhibitors, we have prepared a list of the top 8 items that you should not miss at Automatica 2014.
A lot of robot manufacturers, new and old ones, are launching collaborative robots for Automatica. All these industrial robots will be incorporated into our e-book on collaborative robot, as soon as we have enough information and user feedback.
The Swiss company Mabi will present their brand new collaborative robot. This company is known for its big robotic industrial applications, they decided to level up and add a collaborative robot to their collection. We don’t have a lot of information on this new robot, but at first glance it reminded us of the collaborative robots from Universal Robots. This launch is very exciting, because having another collaborative robot on the market should mean that the price of all these robots will definitely drop as more and more robot manufacturers develop their own models. At the same time, we are working to get some user feedback for you as soon as possible.
The company Gomtec (former RG Mechatronics) will launch a new lightweight robot. Roberta is a lightweight robot with a built-in gripper and intuitive programming software. The interesting thing about Roberta is that its payload to weight ratio is impressive. At only 19 kg, it can handle an 8 kg payload. These features makes it easy to move around the plant or lab and it can still be used for a large array of applications. Roberta will also be available in 3 models: P40.600, P80.800, and P12.1200. You should definitely take a look at Gomtec's website as there are a lot of interesting devices that are also present on the robot arm.
The robot manufacturer F&P Personal Robotic seems to be very focused on small collaborative robots. The company hasn’t provided a lot of information about the P-Rob robot, but the available information tells us that the robot is supposed to be very easy to program with a user-friendly interface. The robot also has its own pincher style gripper. Since the opening on the robot gripper is quite large (60 deg.), it can handle large things such as 1.5L water bottle. As the company is supposed to launch at Automatica, we don’t have any user feedback yet.
We are really looking forward to this show. All of our Robot Grippers will be exhibited at Hall A4, Booth 311, including: the 2-Finger Adaptive Robot Gripper - 200 that has been designed for heavy industrial use, the 2-Finger Adaptive Robot Gripper - 85 that is designed for a lighter charge and collaborative applications, and the 3-Finger Adaptive Robot Gripper that is more versatile with its third finger which can perform more tasks than its two brothers.
Collaborative welding. One of the things that scares managers when it’s time to talk about automated welding is programming time. As with Kinetiq Teaching, this technology aims at reducing downtime due to robot programming. This solution would also enable an operator with less welding knowledge to program a welding robot. The development of this technology shows how making robotic welding programming easier is an issue in the industry.
Cooperative dual arm robot. As robotics is the technology of the future, companies are trying to incorporate dual arm robots (instead of single arm robots) into their assembly line.
Easy automation of assembly tasks. This project looks towards democratizing the assembly tasks of SMEs. In fact, since most of the automated assembly lines are reserved for big international businesses, this project works to allow SMEs to have automated assembly tasks also. Due to the SME's small pool of parts, it is easy for the robot to learn how to assemble the final product.
Pick and place robot. This project includes a robot that assists a specialist in fancy tasks. As the robot can not do the specialized work, it is more like a handyman or an apprentice. You make it do the tasks that you don’t really want to to do or that doesn't require much skill. Apparently this project has such a short setup time that even ten repetitions of task would be worth teaching the robot.
Collaborative machining. Using 2 different kinds of robots that can learn from their past experiences can be useful in machining. Since robots can calibrate themselves and learn, it is a good way to reduce mass production while avoiding incorrect programming.
Intuitive robot interfaces. Most robots are quite hard to program, however, this device allows you to have access to an easy programming method.
The Service Robotics Masters is designed to promote the emerging service robotics market by eliciting and rewarding commercial products and start-up companies. Six finalists have been selected for the final round which takes place at Automatica. Among the finalists let's mention Artiminds Robotics GmbH - coexhibitor with Robotiq - who has developed a software that makes programming of complex robot manipulator motions fast and intuitive. The 2-Finger Adaptive Robot Gripper- 85will be featured in this demonstration. Drop by Hall A4, Booth 235E to meet the finalists and don't forget to attend the award ceremony on Wednesday, June 4th at 4:15 pm.