In the world of robotics, the abbreviation “IP” is often use and can easily be a source of confusion. From Industrial Protocol to Intellectual Property, it is important to distinguish the different meanings of the term “IP”.
Industrial Protocol is a programming language use for communicating with different robotic devices. You will find more information in this article: What Are The Communication Protocols Used In Industrial Robotics?
This protocol is the main communication protocol for data transmissions across network boundaries. It enables internetworking and is the basis for the internet as we know it. More information can be found here: Internet Protocol.
This “IP” is a legal concept that protects the development of something like an idea or an object and gives exclusive rights to its creator. It is often mentioned when talking about inventions or creations. For more information, follow this link: Intellectual Property.
The first number stands for solid particle protection and the second one stands for ingress water protection.
A lot of robot and robotic grippers datasheets contain this information. These classifications are obtained by doing specific tests to insure that the device respects the specifications. It is very useful to determine whether or not the robot can withstand a particular work environment or do certain tasks such as welding, painting or underwater tasks without risking any damage. If the information cannot be easily found, do not hesitate to ask your robot supplier.