The decision has been made to automate a manual handling process. The automation concept has been chosen. Now is time to look into the details on how we will pick, hold and place those parts. The cost of the gripping units itself is not a big part of an automation project. Suction cups can be as little as $10 and an electric gripper can be several $1,000; but these costs represent a small fraction of the whole project. That is why grippers are too often the last aspect to be analyzed in an automation project. But grippers have a direct impact on cell performance and throughput. When budgeting and choosing grippers, it is important to consider performance, purchase cost and even more importantly recurring costs that will come from using the gripper in production. Let's assume that you have analyzed the performance of different gripping options and now want to analyze which one will be the most cost-effective. This article explains how to compare the cost difference between robot gripper options for your automation project.
The following numbers will come into play when comparing the costs of different robot grippers:
For all the options in front of you, define what you will have to purchase initially:
What will be the financial impact of the gripper choice once in production?
What will be the financial impact of the gripper choice if you want to add new products on this line? This aspect is the most difficult to evaluate accurately. Still, it is worth considering it as it can represent large hidden costs. The same costs that were considered at purchase need to be considered here. One difference though is that the programming time will most probably involve stopping the cell production, which can also be quite costly.
I hope that this article showed you the importance of taking the time to analyze which gripper solution is the most cost effective. To help you make the right decision and compare the cost of different gripping options, download our ROI calculator.