The parts are not the important aspect of a network but, rather, how they are interconnected. This is, in fact, the idea behind industrial clusters. They try to build bridges between stakeholders who would not otherwise communicate with each other. The goal is to ideally create a critical mass of interactions among the factions so that the phenomenon becomes self-sustaining. CRIAQ is one such cluster. It brings together players from the Quebec aerospace sector: large companies, SMEs, universities, research centers and students. Events and funding are provided to foster collaborations. I spoke this week with Clément Gosselin (Laval University Robotics Lab), Martin Duchaîne (TechnoMontréal) and my colleagues at Robotiq about creating such an organization for robotics in Quebec. Here’s a summary of our discussion:
Like computers, robots can be used as a tool in various fields. It would therefore be helpful to have an official organization to foster interactions with sectors like medicine, the military, aerospace, manufacturing, rehabilitation, etc. This is when truly interesting applications can arise.
Keeping with the comparison tovideo games and aerospace, robotics has an added attraction: it can contribute directly to the competitive edge of all sectors of our economy, especially manufacturing. Quebec is fortunate to have a strong and diversified manufacturing sector. However, it is precarious at the moment, especially because other countries compete with a labour force that is paid an order of magnitude less. This gap will only grow over the next five to ten years as an aging demographic significantly shrinks the labour market. Many Quebec enterprises won’t survive without robotics. Today, the robot to worker ratio in Canada is less than in most other industrialized countries. We have some serious catching up to do. In addition, today’s robots aren’t made to handle the small to medium-sized runs that are typical of our companies. A real opportunity exists to develop technologies that we can export and use here as well.
A final point favouring a Quebec robotics hub is the recruitment of students for careers in science and engineering. Nowadays, robotics is attracting young people more than any other engineering field. This hub can adopt a mission to develop introductory robotics programs at the secondary and CEGEP levels that prepare students for all engineering fields.
This is all well and good, but it needs to get done. Here are some challenges that we can already identify:
Robotics clusters have already formed naturally around the major American laboratories (Boston/MIT, Pittsburgh/Carnegie Mellon, Silicon Valley/Stanford). The sooner this kind of organization gets off the ground, the better its chances. We can still reach a critical mass and take advantage of our proximity with them. Who’s on board?