In welding, jigs are used to precisely and firmly position parts while they are welded. The picture below shows such a jig.
Welding jigs are typically custom made, per application. With such customization in industrial settings, jigs often come with the following issues:
So if these issues exist, why are jigs still used in robotic welding? The first reason is because jigs have been the industry standard for many years. The second reason is because it is technically challenging to replace them. This is especially true when there are a high number of different parts to weld. In this video (demo was also presented at Fabtech 2010), Fanuc presents a way to use robots that place parts on a simplified jig while other robots do the welding.
Components it takes to create this application:
From our point of view, this is a very promising way to simplify jigs in order to add flexibility, reduce scrap, improve throughput and add flexibility.
If you are looking for ways to simplify jigs in robotic welding, click here to get our ROI calculator and learn how much money you could start saving with such a robotic welding cell solution.