Blog | Robotiq

Presenting the new ActiveDrive toolbar for Universal Robots

Written by Catherine Bernier | May 02, 2016 3:00 PM

Robotiq is proud to launch a new software for Universal Robots: the ActiveDrive toolbar. Robotiq's ActiveDrive toolbar is an add-on software package developed to enhance the guiding mode on Universal Robots. It allows the robot to be moved smoothly and easily to a waypoint.

This add-on is presented in the form of a toolbar located at the top of the UR teach pendant. You can activate and deactivate the ActiveDrive mode from anywhere you are in the Polyscope tabs - simply tap the ActiveDrive button.


Watch the video below to see how it works: 

 

Once ActiveDrive is activated, you'll be able to preset robot movements to help you get to your waypoint.

  • 6-axis movements; which are similar to the actual freedrive mode of UR,
  • Scara movement; allowing translations in the X, Y, Z plane and 1 rotation of the tool,
  • Translation movements; also known as Cartesian movements, which only allow linear translation in the 3 axes,
  • Plane movements; which keep your tool always in the same plan,
  • Automatic tool orientation in the closest orthogonal axis,
  • Speed of the movements (fast or slow).

All of these new features are meant to facilitate the hand guiding of the UR robots. ActiveDrive takes full advantage of the FT-300 and FT-150 for a smoother and more precise movement allowing the robot to be easily moved with only 1 hand.

This new Robotiq product is compatible with UR robots using CB3 and CB3.1 controllers (Polyscope version 3.2 or latest).