As we see trends in collaborative robots users shaping up, we have notice several major distinctions you might be interested in. There is the ''workshop'' user that buys a collaborative robot because it is easy to use and to integrate, especially since there is no need to have a complex programming background or safety guarding. The other ''classic'' user would be the global company that is integrating these devices because they will help liberate time on a large scale once the applications have been developed. In this second case, the major concern for the company is not the programming or integration issue, it is more a question of finding the right application to save time/money/energy on a global scale and being able to automate a simple task that can be replicated in many plants all over the world.
You may ask what is the point of integrating a collaborative robot in a plant such as Volkswagen to automate a simple task? Considering the fact that global companies are able to buy a bunch of industrial robots to weld, paint, assemble and transport cars for example. Why would such a big company be interested in using a robot that is smaller, less precise, slower and with a lower payload?
Repetitive tasks then reinforce the two first reasons for integrating a cobot, it is safe for the human to work alongside the robot and it can help the human to execute tasks that may be inappropriate for him.
If you start to compare collaborative robots with industrial robots you can't really declare a winner or a loser. It highly depends on the applications you want to execute that will decide your robot choice. However, there is a lot of difference in terms of hardware and software between the two kinds of robots.
Industrial Robots: Baseline, the robot is not designed to be safe. It is made to be fast, strong and repetitive. It can't work alongside humans (except under certain conditions) because of the safety guarding that must be in place around it. The robot is made with rectangular shaped parts, that have pinch points and exposed motors. Most of these robots do not have force sensing so they cannot detect if they hit something. These robots have to be programmed with classic programming methods (coding).
In a huge plant, integrating industrial robots can be complex. Production lines may have to be switched and you may have to rethink the position and the purpose of some machines. Notice that these robot can have small to gigantic payloads and/or reach. They also have a wide speed range to provide fast cycle times.
Collaborative Robots: These fellas are designed to work in collaboration with humans. Their general geometry is composed of round shapes. The robot has limited or no pinch points and everything is integrate into the robot frame. All collaborative robots have force sensors in their joints, so they can ''feel'' force applied on them by an external source (impact). Thanks to these force sensors, the robots can be programmed using hand guiding.
Collaborative robots can be integrated at an existing workshop without any significant modifications. Notice that these robots usually have small payloads and reach (except for the new Fanuc CR-35iA).
We recently put together a comparison grid on the difference between collaborative and industrial robot specifications. Take a look at it to see the clear difference between the two devices.
Now that you’re convinced, how can you take advantage of collaborative robots in your workshop?
If you want to learn more about the different types of collaborative robots, I recommend you take a look at our comparison grid on cobots. This grid regroups most collaborative robots on the market today and will help you figure out the different specs you need to look at for your application.