What's the best way to automate a sanding task? Material removal is vital for many manufacturing processes, but it take a lot of time and effort when done manually. There are 3 main ways to automate sanding tasks.
In many manufacturing processes, sanding is one of those tasks that is absolutely vital for achieving a quality product… but also can be a nuisance. Performing sanding tasks manually takes a lot of time and effort, and can be extremely dull (one of the "3 D's of robotic-suitable tasks: dull, dirty and dangerous). What's worse, even in the hands of the most skilled sanding professional there can still be inconsistencies in the quality of the sanding.
Automation can help to improve sanding tasks by doing them faster, with less human intervention, and with much better consistency.
Does that sound good to you?
Would you like to use sanding automation in your business?
Do you have task you think could be improved by automated sanding?
Unfortunately, your decisions aren't over yet. You see, there is more than one way to automate a sanding task. Which option you choose will dramatically influence the effectiveness of your automation effort.
There are three main ways to automate sanding tasks. Let's look at the pros and cons of each.
The "powerhouse" option for sanding is automatic sanding machines. These have been around for a long time and are used in high-volume production environments.
Automatic sanding machines work in the following way:
There are a range of different types of automatic sanding machine, depending on the needs of the task including:
Automatic sanding machines are certainly a reliable option in large-scale production environments. However, there are some advantages and disadvantages to using them.
Advantages include:
Disadvantages include:
A more flexible solution is to use industrial robots for the sanding task. These are able to handle a more varied selection of workpiece sizes and shapes.
There are two ways to achieve industrial robot sanding.
The programming of industrial robot sanding can be quite complex because it requires force control. It can also take a long time to program the waypoints for these tasks, especially when sanding over curved surfaces.
Industrial robot sanding removes some of the inflexibility which is inherent in automatic sanding machines. However, they also have their advantages and disadvantages.
Advantages include:
Disadvantages include:
The final option is collaborative robot sanding. As the name suggests, this involves using a collaborative robot instead of an industrial robot.
Many people believe that collaborative robots are not suitable to tasks like sanding. However, this is not true and one of our newest additions to the Robotiq family of solutions is testament to that — our Sanding Kit for UR robots now makes it easier than ever to automate your sanding task.
Collaborative robot sanding can use both of the two methods that we introduced when we were talking about industrial robot sanding:
However, unlike with industrial robots, collaborative robots are much easier to program for sanding tasks. With our Sanding Kit, you can program a sanding operation in a matter of a few minutes (even for curved surfaces) instead of the hours it could take with an industrial robot. You can even program the robot with hand guiding via the ActiveDrive.
Collaborative robots bring the power of automated sanding into the hands of anyone who wants to use it, without all the cost, size, and complexity of the previous options. Of course, they still have a few advantages and disadvantages.
Advantages include:
Disadvantages include:
Ultimately, the best option for your sanding application will depend on the specific needs of your task. However, now that you have an understanding of the three main options for automated sanding you can make the best choice for you!
Which option sounds best for your application? Tell us in the comments below or join the discussion on LinkedIn, Twitter, Facebook or the DoF professional robotics community.