Skip to content
English
  • There are no suggestions because the search field is empty.

What is the version of my TM Robot ?

There is a big differents between the TM and TM Serie S. That's why it's important to determine what is the version of your robot. 

There is 2 Hardwares versions of the TM robot :

TM : older generation (HW 3.2)

Software version up to the 1.88 ( cannot be updated to the 2.X versions for now )

At the wrist, only I/O available

 

TMS : newer génération (HW 5.0)

Software version to a minimum of 2.0

At the wrist, I/O and Serial communication available.

The look of the robot is different to the previous one (the joint covers are black instead of grey for example)

 

Also the model (TM or TMS) is written directly on the nameplate on the cobot base.