Skip to content
English
  • There are no suggestions because the search field is empty.

Using the Piab Kenos KSG Gripper for Bag Handling

Ensure bag compatibility with the KSG gripper and understand when customer testing is required

Context: The Piab Kenos KSG gripper is commonly used in bag-handling applications, particularly in palletizing cells. This article outlines which bag types are compatible with the KSG and explains the importance of testing customer-supplied bags.

Information:

  1. What is the KSG Gripper?

    • The Piab Kenos KSG is a foam-based vacuum gripper designed for handling flexible packaging.

    • It is commonly integrated into Robotiq palletizing solutions for lifting bags during automated operations.

  2. Bag Compatibility

    • The KSG gripper is compatible with plastic bags and plastic-lined bags.

    • It may not work reliably with:

      • Paper bags

      • Woven sacks

      • Fabric or porous materials

    • The grip depends on the surface's air tightness and structure.

  3. Testing Procedure

    • Robotiq performs validation tests on customer-supplied bags before confirming compatibility.

    • Customers must send representative samples for evaluation.

    • The testing process helps determine if the vacuum system can maintain a reliable grip.

  4. Best Practices

    • Use clean, undamaged bags that maintain their shape.

    • Avoid materials that are porous or that wrinkle easily.

    • Contact Robotiq support early in your integration process to schedule testing.

Conclusion: The Piab Kenos KSG gripper is an effective tool for handling plastic or plastic-lined bags. Due to variability in bag materials, Robotiq requires compatibility testing for customer-specific applications. Reach out to Robotiq to initiate testing and ensure a reliable setup.