How to Program Rigid Interlayers Using the Multipick Feature
Learn how to create and configure rigid interlayers, adjust the gripper model, and use a template program in Robotiq’s Palletizer.
To manage interlayers and see it in the interface, you need to :
1. Create the “interlayer” box using multipick feature
2. Configure the interlayer
3. Replace the automatic gripper model with a custom collision model
You will also find in this article :
4. Programming concept
5. Template program link
1. Create the " box interlayer" using the multipick features




2. how to configure Interlayer:
optional :
Contact detection can be used especially if you interlayer is mid soft. It will allow to bring interlayer above the target with an offset :
- If needed, here is a complete video describing multipick and for more info we recommand using our user manual available on our website.
3. Replace the Automatic Gripper Model with a Custom One

Configure it. X, Y, Z are in the tool referential.

4.Understand the Programming Concept
In this example :
5. Program template for Rigid interlayers
here the link