Stop Conveyor When a Box Is Present at the Input
This article explains how to modify your palletizing program to stop the input conveyor when a box is detected by the input sensor.
Stopping the conveyor can be useful to:
- Prevent other boxes from pushing against the one being picked.
- Save energy by stopping the conveyor when it's not needed.
Implementation
To achieve this, you can add a thread in your palletizing program to continuously monitor the input sensor.
- When a box is detected, the thread stops the conveyor.

- At the end of the thread, the script command sync() is executed to synchronize the thread execution with the main program.