How to change the fingers on a 2F Gripper (C4 Version)?
This article will help you to change the fingers of a 2F85 or a 2F140.
Solution
To replace the fingers of a 2F85 or a 2F140, you will need :
1/- Replacement Fingers
For a 2F85 :
- 1 Replacement Finger: AGC-FIN-085
- 2 Replacement Finger: AGC-FIN-KIT-85-V4
For a 2F140 :
- 1 Replacement Finger: AGC-FIN-140-C4
- 2 Replacement Finger: AGC-FIN-KIT-140-V4
2/- Grease LOCTITE 248
Procedure
1/- Then you will need to remove the screws by using the Allen wrench.

2/- When the screw is removed, you can easily remove the fingers.

3/- Before mounting the new fingers, it's important to make some grease on the screws.
4/- Then you can remount the new fingers. Be carrefull, there is two size of axis.