Skip to content
English
  • There are no suggestions because the search field is empty.

Understanding Accuracy, Repeatability, and Resolution in Robotiq Grippers

Why only position resolution is specified and what it means for your application

This article explains why Robotiq only documents the position resolution of its grippers, such as the 2F-85, and clarifies common misconceptions about accuracy and repeatability in robotic gripping.

What is Position Resolution?

  • Position resolution refers to the smallest detectable movement the gripper can report.

  • For the 2F-85, the total stroke (85 mm) is divided into 256 discrete positions, resulting in a position resolution of approximately 0.4 mm.

  • This means that if the position feedback increases by one unit, the gripper has moved roughly 0.4 mm.

 

Why Repeatability Isn’t Specified

  • Repeatability was once promoted but is no longer documented for the following reasons:

    • Mechanical wear can degrade repeatability over time.

    • Force-based gripping requires travel: about 5 mm of movement is typically needed to achieve reliable grip force.

    • Real-world conditions like speed and force settings influence positioning precision.

  • Because gripping often uses Open/Close commands and requires extra travel for force sensing, the notion of repeatability below 0.4 mm becomes less meaningful.

Feedback Limitations

  • The gripper’s position feedback is not intended as a precise measurement system.

  • The 0.4 mm resolution is a digital step, not a calibrated reference.

  • It should be interpreted as +/-0.2 mm around a nominal position, without a definitive transition point.

 

Calibrate for Better Accuracy

  • Always calibrate the gripper position using a real-world measurement tool (e.g., a ruler).

  • The feedback values are best used for coarse positioning or validation, not for precision measurement.

 

Conclusion: Robotiq grippers offer practical and reliable position feedback, but only resolution is documented due to the complexity and variability of real-world applications. For best results, combine feedback with manual calibration and allow for travel in force-based gripping.