How to control PowerPick on other robot brands ?
PowerPick has been created mainly for Universal Robots and our Palletizing Solution but the product can work with other robot brands.
With PowerPick, it is even simpler than with other products.
Since PowerPick uses solenoid valves, the controls are simple and should work with most robots with 24V and digital I/O. In the manual, there is currently only an example of wiring with a UR robot, but it is easily transposable to another model:

From a mechanical standpoint, PowerPick meets the ISO 9409-1-50-4-M6 tool flange standard. An adapter plate may be required to fit other robot brands.
Here are the SKU available :
- Powerpick 10 : VAC-POWERPICK-KIT
- Powerpick 20 : VAC-POWERPICK20-KIT
- Powerpick 30 : VAC-POWERPICK30-KIT