Skip to content
English
  • There are no suggestions because the search field is empty.

What are the recommandation for the Air supply setup ?

To ensure good performance and reliability, the Screwdriving solution need a proper air supply. Here is an example of such setup.

1. Air supply requirements

The air supply must be dried and filtered according to ISO 8573-1 class 3.4.3.


An air dryer is required on the line.

For the Screwdriving solution air supply pressure should be set between 6.2 bar and 7 bar (90 psi and 100 psi) at the tool with an optimal pressure set at 7 bar (100 psi).

 

2. Proper setup example