Installing the Robotiq Gripper URCap X on Polyscope X
Step-by-step instructions to install the Gripper URCap X on UR’s new Polyscope X platform
This article explains how to install the Robotiq Gripper URCap X on a Universal Robots controller running Polyscope X.
At this time, only the Robotiq Gripper URCapX is available for Polyscope X.
The following Robotiq grippers are compatible with the Gripper URCap X:
- Robotiq Hand-E Gripper
- Robotiq Hand-E C10 Gripper
- Robotiq 2F-85 Adaptive Gripper
- Robotiq 2F-140 Adaptive Gripper
For more details about this URCapX, visit the Robotiq Support Website.
Pre-installation Requirements
Before starting, ensure the following:
-
You are using a UR robot model that supports Polyscope X.
-
The robot is running a compatible version of Polyscope X.
-
You have a USB drive formatted to FAT32.
-
You have downloaded the correct version of the Robotiq Gripper URCapX from the Robotiq website.
Install the URCapX
Follow these steps to install the URCapX on the robot:
-
Insert the USB drive into the UR controller.
-
Power on the robot and launch Polyscope X.
-
Open the Settings menu.
-
Navigate to URCaps.
-
Select Install URCap.
-
Browse to the URCapX file on the USB and select it.
-
Confirm the installation.
-
Once installed, restart Polyscope X if prompted.
Verify the Installation
-
After restarting, go back to Settings > URCaps.
-
Ensure that the Robotiq Gripper URCapX appears in the list.
-
You should now see the Robotiq Gripper icon in the program node options.
Post-Installation Tips
Once the URCapX is installed, Polyscope X will allow you to automatically detect a connected Robotiq Gripper.
To learn more about this process, see the article Automatically Scan for a Robotiq Gripper in Polyscope X.
Conclusion
Installing the Robotiq Gripper URCapX on Polyscope X ensures compatibility with the latest Universal Robots platforms. For additional configuration support or to explore advanced features, refer to the linked resources above.
Need help? Contact Robotiq Support
Updated: June 2026